#include <api/EI_API.h>
void cbGetAttributesAll(EI_API_CIP_NODE_T *pCipNode_p, uint16_t classId_p, uint16_t instanceId_p, uint16_t attrId_p,
EI_API_CIP_SService_t serviceCode_p, int16_t serviceFlag_p)
{
printf("Callback called!\n");
}
uint32_t registerServiceCallback (EI_API_CIP_NODE_T *pCipNode_p)
{
uint32_t errCode;
uint16_t classId = 0x64;
return(errCode);
}
ETHIP_API uint32_t EI_API_CIP_setClassServiceFunc(T *pCipNode_p, uint16_t classId_p, EI_API_CIP_SService_t *pService_p)
Add a callback function to a class service.
Definition: EI_API_CIP_main.c:497
@ EI_API_CIP_eSC_GETATTRIBUTESALL
Definition: EI_API_def.h:114
General service parameter collection.
Definition: EI_API_CIP.h:180