uint32_t EI_API_ADP_setACD | ( | T * | pAdp_p, |
bool | enable_p | ||
) |
Enable or disable address conflict detection (Instance Attribute ID: 10).
Function that allows to enable or disable Address Conflict Detection (ACD).
[in] | pAdp_p | Pointer to the adapter. |
[in] | enable_p | Boolean flag which enables or disables the ACD functionality. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |