uint32_t EI_API_ADP_getEnipAcdHdr | ( | T * | pAdp_p, |
EI_API_ADP_SParam_t * | pEnipAcdHdr_p | ||
) |
Get the adapter address conflict detection header (Instance Attribute ID: 11).
Function to get the current Address Conflict Detection (ACD) header.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pEnipAcdHdr_p | Pointer to the ACD header packed within a EI_API_ADP_SParam_t type. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |