EtherNet/IP™ Adapter  1.02.01
User Reference Manual

◆ EI_API_ADP_setIpTTL()

uint32_t EI_API_ADP_setIpTTL ( T *  pAdp_p,
uint8_t  ipTTL_p 
)

Set the adapter IP TTL value (Instance Attribute ID: 8).

This function can be used to set the current adapter IP Time-to-Live (TTL) value. By default, the TTL value is set to 1. The maximum value for TTL is 255.

Parameters
[in]pAdp_pPointer to the adapter.
[in]ipTTL_pNew TTL value.
Returns
EI_API_ADP_EError_t as uint32_t value.
Return values
EI_API_ADP_eERR_OKSuccess.
EI_API_ADP_eERR_GENERALGeneral error.
Example
#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
pEI_API_ADP = EI_API_ADP_new(numInterfaces);
errCode = EI_API_ADP_setIpTTL(pEI_API_ADP, 1);
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:195
ETHIP_API uint32_t EI_API_ADP_setIpTTL(T *pAdp_p, uint8_t ipTTL_p)
Set the adapter IP TTL value (Instance Attribute ID: 8).
Definition: EI_API_ADP_main.c:2618
See also
EI_API_ADP_getIpTTL EI_API_ADP_EError_t