uint32_t EI_API_ADP_isHwSettingEnabled | ( | T * | pAdp_p, |
bool * | pHwConfigEnabled_p | ||
) |
This function returns the hardware settings.
The function returns true if the hardware settings are enabled. Otherwise false.
[in] | pAdp_p | Pointer to the adapter. |
[out] | pHwConfigEnabled_p | Pointer to a boolean that is set to true if hardware configuration is enabled and false if not. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |