#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:195
ETHIP_API uint32_t EI_API_ADP_setMcastConfiguration(T *pAdp_p, const EI_API_ADP_SMcastConfig_t *pMcast_p)
Set the current Mcast configuration (Instance Attribute ID: 9).
Definition: EI_API_ADP_main.c:2744
General multi-cast attribute parameter collection.
Definition: EI_API_def.h:240