EtherCAT Slave  1.04.01

◆ EC_API_SLV_setInputData()

uint32_t EC_API_SLV_setInputData ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
uint32_t  length_p,
uint8_t *  pInputData_p 
)

Write input process data to the EtherCAT Master.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]length_pdata length in bytes
[in]pInputData_ppointer to data
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
// the Call
retVal = EC_API_SLV_setInputData(ptEcSlvApi, length, data);
EC_API_SLV_setInputData
uint32_t EC_API_SLV_setInputData(EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint32_t length_p, uint8_t *pInputData_p)
Write input process data to the EtherCAT Master.
Definition: ecSlvApi_ProcDataStub.c:798