EtherCAT Slave  1.04.01

◆ EC_API_SLV_cbRegisterBoardStatusLed()

void EC_API_SLV_cbRegisterBoardStatusLed ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
void *  pContext_p,
EC_API_SLV_CBBoardStatusLed_t  cbFunc_p,
void *  pLedContext_p 
)

Register Board Status LED callback.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]pContext_pcall context
[in]cbFunc_pFunction pointer to the FoE Open file Handler
[in]pLedContext_pLED context
Example
#include <theHeader.h>
// required variables
uint32_t retVal = 0;
void* pvVariable = NULL;
// the Call
retVal = void EC_API_SLV_cbRegisterBoardStatusLed(EC_API_SLV_SHandle_t *ecSlaveApi, EC_API_SLV_CBBoardStatusLed_t cbFunc, void* ctxt)(pvVariable);
See also
theReference
Examples
ecSlvCiA402.c, and ecSlvESI.c.
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:134
EC_API_SLV_cbRegisterBoardStatusLed
void EC_API_SLV_cbRegisterBoardStatusLed(EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBBoardStatusLed_t cbFunc_p, void *pLedContext_p)
Register Board Status LED callback.
Definition: ecSlvApi_BoardStub.c:271
EC_API_SLV_CBBoardStatusLed_t
void(* EC_API_SLV_CBBoardStatusLed_t)(void *pContext_p, void *pLedContext_p, bool errLed_p, bool statusLed_p)
Set Status LED call back.
Definition: ecSlvApi.h:847