EtherCAT Slave  1.04.01

◆ EC_SLV_APP_setCiA402ObjectValue()

uint32_t EC_SLV_APP_setCiA402ObjectValue ( EC_API_SLV_SHandle_t pEcApiSlv_p,
uint16_t  index_p,
uint16_t  length_p,
uint16_t *  pValue_p 
)

Write CiA402 Object value.

Remarks
Use OBD indexes described in ETG6010 Chapter 16. axis_p parameter calculates the axis object index.
Parameters
[in]pEcApiSlv_pDTK Instance.
[in]index_pCiA402 Object index.
[in]axis_pAxis number.
[in]length_pObject length.
[in]pValue_pObject Value.
Returns
ErrorCode DTK Error code.
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
uint16_t index;
int16_t* value;
uint8_t axis;
// the Call
retVal = EC_SLV_APP_setCiA402ObjectValue(S_ecSlvApiHdl, index, axis, sizeof(value), &value);
Examples
ESL_cia402Demo.c.
EC_API_SLV_SHandle_t
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:134
EC_SLV_APP_setCiA402ObjectValue
uint32_t EC_SLV_APP_setCiA402ObjectValue(EC_API_SLV_SHandle_t *pEcApiSlv_p, uint16_t index_p, uint16_t length_p, uint16_t *pValue_p)
Write CiA402 Object value.
Definition: ESL_cia402Demo.c:167