Get resource range response message.
Response sent to host processor containing the requested resource range assigned to the host who sent the range request.
The range_start and range_num values are zero if the type and subtype in the range request do not form a unique resource type for the SoC. In this case, the response will still contain an ACK.
- Parameters
-
hdr | Standard TISCI header |
range_start | Start index of retrieved resource range. Zero if the resource is not valid. |
range_num | Number of resources in the range. Zero if the resource is not valid. |
range_start_sec | Start index of retrieved secondary resource range. Zero if the resource is not valid. |
range_num_sec | Number of resources in secondary range. Zero if the resource is not valid. |