Different callbacks which can be registered.
While calling the function set in ICSS_EMAC_CallBack, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (as mentioned in the member descriptions), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig.
ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::port0LinkCallBack |
Callback function for link change on Port 0. Second argument to callback is linkStatus
ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::port1LinkCallBack |
Callback function for link change on Port 1. Second argument to callback is linkStatus
ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::rxNRTCallBack |
Callback function for packets received with queueNumber >= ethPrioQueue (of ICSS_EMAC_Attrs). Second argument to callback is queueNumber.
ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::rxRTCallBack |
Callback function for packets received with queueNumber < ethPrioQueue (of ICSS_EMAC_Attrs). Second argument to callback is queueNumber.
ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::txCallBack |
Callback function for packet Tx completion. Second argument is NULL
ICSS_EMAC_CallBackConfig ICSS_EMAC_CallBackObject::learningExCallBack |
Callback function for protocol specific exception adaptation in learning. Second argument is macId