AM64x MCU+ SDK  08.00.00

Detailed Description

CSL_UdmapTR0 specifies a Type 0 (One dimensional data move) Transfer Request.

Data Fields

uint32_t flags
 
uint32_t icnt0
 
uint64_t addr
 

Field Documentation

◆ flags

uint32_t CSL_UdmapTR0::flags

Specifies type of TR and how the TR should be handled. It also supports the TR triggering and output events.

◆ icnt0

uint32_t CSL_UdmapTR0::icnt0

Total loop iteration count for level 0 (innermost)

◆ addr

uint64_t CSL_UdmapTR0::addr

Starting address for the source data or destination data if it is a half duplex write