![Logo](ti_logo.svg) |
AM64x MCU+ SDK
08.00.00
|
|
Go to the documentation of this file.
56 #define DEFAULT_DLR_PACKET_SIZE 60
58 #define ETHERNET_FRAME_SIZE_60 60
61 #define IEP_WD_PRE_DIV_10US 2000
64 #define PORT0_WATCH_DOG_ID 0
66 #define PORT1_WATCH_DOG_ID 1
68 #define IS_A_LINK_STATUS_FRAME DLR_TRUE
69 #define IS_A_NEIGHBOR_STAT_FRAME DLR_FALSE
72 #define BOTH_LINKS_UP 0x0
73 #define PORT0_IS_DOWN 0x2
74 #define PORT1_IS_DOWN 0x1
75 #define BOTH_LINKS_DOWN 0x3
78 #define PORT0_WD_ISR_MASK 0x2000000
80 #define PORT1_WD_ISR_MASK 0x4000000
86 #define PDI_WD_TRIGGER_RX_SOF (0 << 4)
92 #define PDI_WD_TRIGGER_LATCH_IN (1 << 4)
98 #define PDI_WD_TRIGGER_SYNC0_OUT (2 << 4)
104 #define PDI_WD_TRIGGER_SYNC1_OUT (3 << 4)
107 #define MAX_EVENTS_CAPTURED 1000
110 #define LINK1_BREAK 1
111 #define LINK2_BREAK 2
112 #define BOTH_LINK_DISABLED 3
113 #define EMPTY_SIGNON_FRAME_RCVD 4
114 #define COMPLETE_SIGNON_FRAME_RCVD 5
116 #define RING_FAULT_RCVD_PORT0 6
117 #define RING_FAULT_RCVD_PORT1 7
119 #define RING_FAULT_TRANSITION_PORT0 8
120 #define RING_FAULT_TRANSITION_PORT1 9
122 #define RING_NORMAL_TRANSITION_PORT0 10
123 #define RING_NORMAL_TRANSITION_PORT1 11
125 #define START_TIMER0 12
126 #define START_TIMER1 13
128 #define NCRES_RCVD_PORT0 14
129 #define NCRES_RCVD_PORT1 15
131 #define NCREQ_RCVD_PORT0 16
132 #define NCREQ_RCVD_PORT1 17
134 #define LOCFAULT_RCVD_PORT0 18
135 #define LOCFAULT_RCVD_PORT1 19
137 #define BEACON0_MISSED_FAULT 20
138 #define BEACON1_MISSED_FAULT 21
139 #define BEACON0_MISSED_NORMAL 22
140 #define BEACON1_MISSED_NORMAL 23
142 #define LINK1_FAULT_BREAK 24
143 #define LINK2_FAULT_BREAK 25
145 #define LINK1_NORMAL_BREAK 27
146 #define LINK2_NORMAL_BREAK 28
148 #define NEIGHBOR_TIMEOUT_PORT0_RETRY 29
149 #define NEIGHBOR_TIMEOUT_PORT1_RETRY 30
150 #define NEIGHBOR_TIMEOUT_PORT0_MAX 31
151 #define NEIGHBOR_TIMEOUT_PORT1_MAX 32
153 #define DLR_RESET_MACHINE 33
155 #define BEACON0_MISSED 34
156 #define BEACON1_MISSED 35
158 #define STOP_BOTH_TIMERS_PORT0 36
159 #define STOP_BOTH_TIMERS_PORT1 37
161 #define PORT0_BEACON_STALL 38
162 #define PORT1_BEACON_STALL 39
166 #define DEFAULT_BEACON_INTERVAL_VARIABLE 400
167 #define DEFAULT_BEACON_TIMEOUT_VARIABLE (DEFAULT_BEACON_INTERVAL_VARIABLE * 4)
170 #define DEFAULT_NEIGHBOR_TIMEOUT_INTERVAL 200
173 #define DEFAULT_DLR_PERIODIC_INTERVAL 100
176 #define MAX_NUM_RETRIES 3
179 #define BEACON_CPU_STALL_THRESHOLD 4
184 #define DLR_DEFAULT_CAPABILITIES (1 << 7) | (1 << 1)
187 #define DLR_SIGNON_FRAME_SIZE ICSS_EMAC_MAXMTU
189 #define DLR_COMMON_FRAME_HEADER_SIZE 18
190 #define DLR_COMMON_FRAME_OFFSET 12
193 #define ICSS_DLR_PORT0_INT_FLAG 0x200000
195 #define ICSS_DLR_PORT1_INT_FLAG 0x400000
198 #define DLR_DMTIMER4_ID 3
200 #define DLR_DMTIMER5_ID 4
338 uint8_t supMACAddress[6];
381 #ifdef IS_A_DLR_SUPERVISOR
418 #ifdef IS_A_DLR_SUPERVISOR
420 uint32_t numRingFaultsPowerUp;
423 uint16_t ringParticipantsCount;
432 typedef struct dlr_Config_s
592 uint32_t sequenceId);
609 uint8_t linkOrNeighbor, uint8_t linkStatus);
639 uint8_t portNum, uint16_t
size);
705 void genSeqOfEvents(uint8_t event);
786 uint16_t periodInMicroSec, uint8_t
id);
dlrStruct * dlrObj
Definition: icss_dlr.h:434
uint16_t vLanId
Definition: icss_dlr.h:324
State machine variables, part of DLR Object and L2 implementation.
Definition: icss_dlr.h:294
ClockP_Object dlrPeriodicTimerObject
Definition: icss_dlr.h:448
uint8_t beaconTimeoutIntNum_P0
Definition: icss_dlr.h:413
struct ICSS_EMAC_Config_s * ICSS_EMAC_Handle
Alias for ICSS EMAC Handle containing base addresses and modules.
Definition: icss_emac.h:366
uint16_t size
Definition: tisci_boardcfg.h:1
void EIP_DLR_setTimeout_WD_IEP(EIP_DLRHandle dlrHandle, uint16_t periodInMicroSec, uint8_t id)
Set the timeout value in watchdog.
void EIP_DLR_beaconTimeoutISR_P1(uintptr_t arg)
ISR for beacon timeout for Port 1.
void EIP_DLR_beaconTimeoutISR_P0(uintptr_t arg)
ISR for beacon timeout for Port 0.
void EIP_DLR_stop(EIP_DLRHandle dlrHandle)
API to stop the DLR driver Halt DLR. Calling this disables DLR on the device.
uint8_t supPrecedence
Definition: icss_dlr.h:327
nwStatus
network status : possible values for Attribute ID 2
Definition: icss_dlr.h:242
uint32_t tracePktIntervalCount
Definition: icss_dlr.h:453
void EIP_DLR_enable_WD_IEP(EIP_DLRHandle dlrHandle, uint8_t id)
Enable the IEP Watch dog timers.
@ FEATURE_UNSUPPORTED
Definition: icss_dlr.h:270
uint8_t port0IntNum
Definition: icss_dlr.h:407
PRUICSS_Handle pruicssHandle
Definition: icss_dlr.h:438
@ NODE_NORMAL
Definition: icss_dlr.h:214
uint32_t supIPAddress
Definition: icss_dlr.h:341
Opaque clock object used with the clock APIs.
Definition: ClockP.h:59
nodeState
node state machine states
Definition: icss_dlr.h:208
uint8_t checkForLoop
Definition: icss_dlr.h:452
void EIP_DLR_neighborTimeoutISR1(ClockP_Object *obj, void *arg)
ISR for Neighbor timeout timer for port 1.
void EIP_DLR_processDLRFrame(EIP_DLRHandle dlrHandle, uint8_t *pktBuffer, uint8_t portNum, uint16_t size)
Processes a sign on and Neighbor check request frame.
@ BACKUP_NODE
Definition: icss_dlr.h:261
struct dlr_Config_s * EIP_DLRHandle
Definition: icss_dlr.h:202
#define DEFAULT_DLR_PACKET_SIZE
Definition: icss_dlr.h:56
@ NODE_IDLE
Definition: icss_dlr.h:210
uint16_t deviceNum
Definition: icss_dlr.h:357
int32_t EIP_DLR_isrInit(EIP_DLRHandle dlrHandle)
@ UNEXPECTED_LOOP
Definition: icss_dlr.h:248
uint32_t deviceIP
Definition: icss_dlr.h:440
void EIP_DLR_port1ProcessLinkBrk(uint8_t linkStatus, void *arg2)
Process DLR state machine in the event of a link break on Port1.
HwiP_Object port1IntObject
Definition: icss_dlr.h:402
@ NORMAL_STAT
Definition: icss_dlr.h:244
void EIP_DLR_genNCReqFrame(EIP_DLRHandle dlrHandle, uint8_t *src, uint8_t sourcePort)
supervisorStatus
device role: possible values for Attribute ID 3
Definition: icss_dlr.h:259
HwiP_Object beaconTimeoutIntP0Object
Definition: icss_dlr.h:403
activeSuperAddr addr
Definition: icss_dlr.h:377
uint8_t numExceptions
Definition: icss_dlr.h:286
void EIP_DLR_setDefaultValue(EIP_DLRHandle dlrHandle)
ICSS_EMAC_Handle emacHandle
Definition: icss_dlr.h:435
void EIP_DLR_genNeighborLinkStatFrame(EIP_DLRHandle dlrHandle, uint8_t *src, uint8_t sourcePort, uint8_t linkOrNeighbor, uint8_t linkStatus)
void EIP_DLR_addToExceptionList(EIP_DLRHandle dlrHandle, uint8_t *macId)
@ RING_NORMAL
Definition: icss_dlr.h:222
HwiP_Object beaconTimeoutIntP1Object
Definition: icss_dlr.h:404
void EIP_DLR_addSignOnNumNodes(uint8_t *src, uint16_t numNodes)
void EIP_DLR_switchToNormal(EIP_DLRHandle dlrHandle)
uint8_t port1IntNum
Definition: icss_dlr.h:410
@ RING_NODE
Definition: icss_dlr.h:265
@ RING_TOP
Definition: icss_dlr.h:235
void EIP_DLR_neighborTimeoutISR0(ClockP_Object *obj, void *arg)
ISR for Neighbor timeout timer for port 0.
uint32_t sequenceID
Definition: icss_dlr.h:442
@ RING_FAULT_STAT
Definition: icss_dlr.h:246
uint8_t beaconTimeoutIntNum_P1
Definition: icss_dlr.h:416
Supervisor configuration. Attribute ID 4.
Definition: icss_dlr.h:312
dlrStateMachineVar SMVariables
Definition: icss_dlr.h:379
void EIP_DLR_resetStateMachine(EIP_DLRHandle dlrHandle)
Initialize the state machine when it goes back to idle state.
uint32_t dlrCapabilities
Definition: icss_dlr.h:396
void EIP_DLR_setDivider_WD_IEP(EIP_DLRHandle dlrHandle)
Sets the clock divider to 1us for IEP watch dog timers.
ringState
ring state values
Definition: icss_dlr.h:220
uint8_t superStatus
Definition: icss_dlr.h:304
void EIP_DLR_start(EIP_DLRHandle dlrHandle)
API to start the DLR driver Calling this enables DLR on the device.
uint32_t ipAddr
Definition: icss_dlr.h:365
superConfig supConfig
Definition: icss_dlr.h:375
void EIP_DLR_disable_WD_IEP(EIP_DLRHandle dlrHandle, uint8_t id)
Disable the IEP Watch dog timers.
@ NON_DLR
Definition: icss_dlr.h:267
Definition: icss_dlr.h:433
uint8_t EIP_DLR_checkSupervisorException(uint8_t *macId, EIP_DLRHandle dlrHandle)
void EIP_DLR_init(EIP_DLRHandle dlrHandle)
API to initialize the DLR driver.
void EIP_DLR_clearExceptionList(EIP_DLRHandle dlrHandle)
uint8_t status
Definition: icss_dlr.h:302
void EIP_DLR_port1ISR(uintptr_t arg)
Fast ISR for Port 1, bypasses the buffer copy and NDK.
void EIP_DLR_switchToFault(EIP_DLRHandle dlrHandle)
uint8_t topology
Definition: icss_dlr.h:300
char mode[32]
Definition: tisci_pm_core.h:1
List of MAC ID's which are exempted from Learning, this is for DLR implementation.
Definition: icss_dlr.h:282
nwTopology
network topology : possible values for Attribute ID 1
Definition: icss_dlr.h:231
@ NODE_FAULT
Definition: icss_dlr.h:212
uint8_t activeSuperPred
Definition: icss_dlr.h:399
IP and MAC of the Ring devices. Attribute ID 9.
Definition: icss_dlr.h:364
HwiP_Object port0IntObject
Definition: icss_dlr.h:401
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:91
@ RAPID_FAULT
Definition: icss_dlr.h:252
uint32_t beaconTimeout
Definition: icss_dlr.h:321
Last active node at the end of the chain Class for Attributes 6 and 7.
Definition: icss_dlr.h:350
void EIP_DLR_initDLRFrameHeader(uint8_t *src, uint8_t *header)
uint32_t ipAddr
Definition: icss_dlr.h:352
exceptionList * exclusionList
Definition: icss_dlr.h:444
uint8_t pktSendCounter
Definition: icss_dlr.h:455
@ RING_FAULT
Definition: icss_dlr.h:224
void EIP_DLR_addModuleIPAddress(EIP_DLRHandle dlrHandle, uint32_t newIP)
uint8_t node_state
Definition: icss_dlr.h:296
uint32_t beaconInterval
Definition: icss_dlr.h:319
@ ACTIVE_RING_SUPERVISOR
Definition: icss_dlr.h:263
void EIP_DLR_periodicProcessing(ClockP_Object *obj, void *userArg)
uint8_t superEnable
Definition: icss_dlr.h:317
DLR parent structure through which all other structures can be accessed.
Definition: icss_dlr.h:373
void EIP_DLR_set_pdi_wd_trigger_mode(EIP_DLRHandle dlrHandle, uint32_t mode)
Set the PDI WD trigger mode.
struct PRUICSS_Config_s * PRUICSS_Handle
A handle that is returned from a PRUICSS_open() call. This handle is required for calling other APIs.
Definition: pruicss/v0/pruicss.h:234
Supervisor address, part of DLR Object. Attribute ID 10.
Definition: icss_dlr.h:335
uint32_t stateMachineCount
Definition: icss_dlr.h:454
uint8_t ring_state
Definition: icss_dlr.h:298
void EIP_DLR_port0ISR(uintptr_t arg)
Fast ISR for Port 0, bypasses the buffer copy and NDK.
@ PARTIAL_FAULT
Definition: icss_dlr.h:250
void EIP_DLR_genNCResFrame(uint8_t *src, uint8_t sourcePort, uint8_t reqSrcPort, uint32_t sequenceId)
void EIP_DLR_port0ProcessLinkBrk(uint8_t linkStatus, void *arg2)
Process DLR state machine in the event of a link break on Port0.
void EIP_DLR_dRAMInit(EIP_DLRHandle dlrHandle)
void EIP_DLR_addVlanID(uint8_t *src, uint16_t vlanID)
#define ICSS_EMAC_MAX_PORTS_PER_INSTANCE
Maximum number of Ports in a single ICSS
Definition: icss_emac.h:66
@ LINEAR_TOP
Definition: icss_dlr.h:233