See IPC Notify for more details.
|
| typedef void(* | IpcNotify_FxnCallback) (uint32_t remoteCoreId, uint16_t localClientId, uint32_t msgValue, void *args) |
| | User callback that is invoked when a message is received from a reote core for a given client ID. More...
|
| |
◆ IPC_NOTIFY_CLIENT_ID_MAX
| #define IPC_NOTIFY_CLIENT_ID_MAX (16U) |
Maximum number of clients possible for receiving messages.
◆ IPC_NOTIFY_CLIENT_ID_RPMSG
| #define IPC_NOTIFY_CLIENT_ID_RPMSG (0U) |
Client ID used by rpmessage, this client ID should not be used by other users.
◆ IPC_NOTIFY_CLIENT_ID_SYNC
| #define IPC_NOTIFY_CLIENT_ID_SYNC (1U) |
Client ID used for sync messages, this client ID should not be used by other users.
◆ IPC_NOTIFY_MSG_VALUE_MAX
| #define IPC_NOTIFY_MSG_VALUE_MAX (0x10000000U) |
Maximum value of message that can be sent and received.
◆ IpcNotify_FxnCallback
| typedef void(* IpcNotify_FxnCallback) (uint32_t remoteCoreId, uint16_t localClientId, uint32_t msgValue, void *args) |
User callback that is invoked when a message is received from a reote core for a given client ID.
Before invoking the API, the IPC module would have 'popped` the message from the HW or SW FIFO already. This callback is called frm ISR context, so all constraints of ISR should be applied by the callback, e.g. no blocking wait, quickly handle message and exit ISR.
For most applications, it is recommended to put the message value into a local SW queue and defer the message handling itself to a application task.
- Parameters
-
| remoteCoreId | [in] Remote core that has sent the message |
| localClientId | [in] Local client ID to which the message is sent |
| msgValue | [in] Message value that is sent |
| args | [in] Argument pointer passed by user when IpcNotify_registerClient is called |
◆ IpcNotify_Params_init()
Set default value to IpcNotify_Params.
- Parameters
-
| params | [out] Default initialized structure |
◆ IpcNotify_init()
Initialize IPC Notify module.
This API will initialize the HW used for IPC including registering interrupts for receiving messages.
- Parameters
-
| params | [in] Initializaion parameters |
◆ IpcNotify_deInit()
| void IpcNotify_deInit |
( |
| ) |
|
De-initialize IPC Notify module.
This API will de-initialize the HW used for IPC including un-registering interrupts for receiving messages.
◆ IpcNotify_sendMsg()
| int32_t IpcNotify_sendMsg |
( |
uint32_t |
remoteCoreId, |
|
|
uint16_t |
remoteClientId, |
|
|
uint32_t |
msgValue, |
|
|
uint32_t |
waitForFifoNotFull |
|
) |
| |
Send message to a specific remote core and specific client ID on that remote core.
- Note
- To reduce latency, error checks are avoided in this API. Users need to make sure the client ID value is < IPC_NOTIFY_CLIENT_ID_MAX and message value is < IPC_NOTIFY_MSG_VALUE_MAX
-
This API can be called from within ISRs and is also thread-safe. Internally this API disables interrupts for a short while to make the API ISR and thread safe.
-
One cannot send messages to self, i.e remoteCoreId, cannot be same as core ID of the CPU that called this API.
- Parameters
-
| remoteCoreId | [in] Remote core to sent message to, see CSL_CoreID for valid values. |
| remoteClientId | [in] Remote core client ID to send message to, MUST be < IPC_NOTIFY_CLIENT_ID_MAX |
| msgValue | [in] Message value to send, MUST be < IPC_NOTIFY_MSG_VALUE_MAX |
| waitForFifoNotFull | [in] 1: wait for message to be inserted into HW or SW FIFO, 0: if FIFO is full, dont send message and return with error. |
- Returns
- SystemP_SUCCESS, message sent successfully
-
SystemP_FAILURE, message could not be sent since HW or SW FIFO for holding the message is full.
◆ IpcNotify_registerClient()
| int32_t IpcNotify_registerClient |
( |
uint16_t |
localClientId, |
|
|
IpcNotify_FxnCallback |
msgCallback, |
|
|
void * |
args |
|
) |
| |
Register a callback to handle messages received from a specific remote core and for a specific local client ID.
- Parameters
-
| localClientId | [in] Client ID to which the message has been sent |
| msgCallback | [in] Callback to invoke, if callback is already registered, error will be returned. |
| args | [in] User arguments, that are passed back to user when the callback is invoked |
- Returns
- SystemP_SUCCESS, callback registered sucessfully
-
SystemP_FAILURE, callback registration failed, either remoteCoreId or localClientId is invalid or callback already registered.
◆ IpcNotify_unregisterClient()
| int32_t IpcNotify_unregisterClient |
( |
uint16_t |
localClientId | ) |
|
Un-register a previously registered callback.
- Parameters
-
| localClientId | [in] Client ID to which the message has been sent |
- Returns
- SystemP_SUCCESS, callback un-registered sucessfully
-
SystemP_FAILURE, callback un-registration failed, either remoteCoreId or localClientId is invalid
◆ IpcNotify_getSelfCoreId()
| uint32_t IpcNotify_getSelfCoreId |
( |
| ) |
|
Return current core ID.
- Returns
- Core ID, see CSL_CoreID for valid values.
◆ IpcNotify_isCoreEnabled()
| uint32_t IpcNotify_isCoreEnabled |
( |
uint32_t |
coreId | ) |
|
Check if a core is enabled for IPC.
- Parameters
-
| coreId | [in] Core ID, see CSL_CoreID for valid values. |
- Returns
- 1: core is enabled for IPC, 0: core is not enabled for IPC
◆ IpcNotify_sendSync()
| int32_t IpcNotify_sendSync |
( |
uint32_t |
remoteCoreId | ) |
|
Send a sync message to specific core.
This API can be used to send sync message's to very specific core's For most users recommend to use the more simpler IpcNotify_syncAll() API.
- Parameters
-
| remoteCoreId | [in] Core ID, see CSL_CoreID for valid values. |
- Returns
- SystemP_SUCCESS, sync message was sent successfully, else failure
◆ IpcNotify_waitSync()
| int32_t IpcNotify_waitSync |
( |
uint32_t |
remoteCoreId, |
|
|
uint32_t |
timeout |
|
) |
| |
Wait for a sync message to be received from the specified core.
This API can be used to recevice sync message from very specific core's For most users recommend to use the more simpler IpcNotify_syncAll() API.
- Parameters
-
| remoteCoreId | [in] Core ID, see CSL_CoreID for valid values. |
| timeout | [in] Amount of time in units of ticks to wait |
- Returns
- SystemP_SUCCESS, sync message was recevied successfully
-
SystemP_TIMEOUT, sync message was NOT recevied after
timeout ticks
-
SystemP_FAILURE, invalid arguments
◆ IpcNotify_syncAll()
| int32_t IpcNotify_syncAll |
( |
uint32_t |
timeout | ) |
|
Send a message to all enabled cores and wait for sync message from all enabled cores.
This API when called on all CPUs, make sure all CPUs execute upto a certain and then proceed only when all other CPUs have also executed to the same point.
This is useful esp during system init to make sure message exchange can be started only after all CPUs have finished their system initialization.
- Parameters
-
| timeout | [in] Amount of time in units of ticks to wait for the sync |
- Returns
- SystemP_SUCCESS, all sync messages recevied successfully
-
SystemP_TIMEOUT, some sync messages was NOT recevied after
timeout ticks
-
SystemP_FAILURE, invalid arguments