AM62x MCU+ SDK  09.02.01

Detailed Description

Get resource range response message.

Response sent to host processor containing the requested resource range assigned to the host who sent the range request.

The range_start and range_num values are BOTH zero if the type and subtype in the range request do not form a unique resource type for the SoC. In this case, the response will still contain an ACK.

Parameters
hdrStandard TISCI header
range_startStart index of retrieved resource range.
range_numNumber of resources in the range. Zero if the resource is not valid.
range_start_secStart index of retrieved secondary resource range. Zero if a second resource range does not exist or if the resource is not valid.
range_num_secNumber of resources in secondary range. Zero if a second resource range does not exist or if the resource is not valid.

Data Fields

struct tisci_header hdr
 
uint16_t range_start
 
uint16_t range_num
 
uint16_t range_start_sec
 
uint16_t range_num_sec
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_rm_get_resource_range_resp::hdr

◆ range_start

uint16_t tisci_msg_rm_get_resource_range_resp::range_start

◆ range_num

uint16_t tisci_msg_rm_get_resource_range_resp::range_num

◆ range_start_sec

uint16_t tisci_msg_rm_get_resource_range_resp::range_start_sec

◆ range_num_sec

uint16_t tisci_msg_rm_get_resource_range_resp::range_num_sec