AM62x MCU+ SDK  09.02.01

Detailed Description

Request for retrieving the firewall permissions.

Parameters
hdrGeneric TISCI message header.
fwl_idfirewall ID in question. fwl_id is defined in the TRM.
regionRegion or channel number to set config info

This field is unused in case of a simple firewall and must be initialized to zero. In case of a region based firewall, this field indicates the region in question (index starting from 0). In case of a channel based firewall, this field indicates the channel in question (index starting from 0).

Parameters
n_permission_regsNumber of permission registers to retrieve

Data Fields

struct tisci_header hdr
 
uint16_t fwl_id
 
uint16_t region
 
uint32_t n_permission_regs
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_fwl_get_firewall_region_req::hdr

◆ fwl_id

uint16_t tisci_msg_fwl_get_firewall_region_req::fwl_id

◆ region

uint16_t tisci_msg_fwl_get_firewall_region_req::region

◆ n_permission_regs

uint32_t tisci_msg_fwl_get_firewall_region_req::n_permission_regs