AM62x MCU+ SDK  12.00.00

Detailed Description

PHY driver FSM state.

Data Fields

EnetPhy_FsmState fsmState
 
bool fsmStateChanged
 
EnetPhy_Speed speed
 
EnetPhy_Duplexity duplexity
 
uint32_t timeout
 
uint32_t residenceTime
 
bool isNwayCapable
 
bool enableNway
 
bool needsManualCfg
 
bool needsNwayCfg
 
uint32_t linkCaps
 
uint32_t phyLinkCaps
 
bool loopbackEn
 
bool needsMdixSwitch
 
bool enableMdix
 

Field Documentation

◆ fsmState

EnetPhy_FsmState EnetPhy_State::fsmState

PHY state-machine state

◆ fsmStateChanged

bool EnetPhy_State::fsmStateChanged

Whether the PHY state-machine state has changed

◆ speed

EnetPhy_Speed EnetPhy_State::speed

PHY speed (auto-negotiated or manually set)

◆ duplexity

EnetPhy_Duplexity EnetPhy_State::duplexity

PHY duplexity (auto-negotiated or manually set)

◆ timeout

uint32_t EnetPhy_State::timeout

Timeout (ticks)

◆ residenceTime

uint32_t EnetPhy_State::residenceTime

Residence time (ticks)

◆ isNwayCapable

bool EnetPhy_State::isNwayCapable

Whether PHY is auto-negotiation capable

◆ enableNway

bool EnetPhy_State::enableNway

Whether auto-negotiation is to be used or not

◆ needsManualCfg

bool EnetPhy_State::needsManualCfg

Whether manual mode needs to be configured

◆ needsNwayCfg

bool EnetPhy_State::needsNwayCfg

Whether auto-negotiation advertisement needs to be configured

◆ linkCaps

uint32_t EnetPhy_State::linkCaps

Refined link capability mask (app, SoC, PHY)

◆ phyLinkCaps

uint32_t EnetPhy_State::phyLinkCaps

PHY link capability mask

◆ loopbackEn

bool EnetPhy_State::loopbackEn

Whether PHY loopback is enabled or not

◆ needsMdixSwitch

bool EnetPhy_State::needsMdixSwitch

Whether MDIX switch is needed or not

◆ enableMdix

bool EnetPhy_State::enableMdix

Whether MDIX is enabled or not (MDI)