AM62x MCU+ SDK  12.00.00
Dss_DctrlVpSafetyChkParams Struct Reference

Detailed Description

Structure containing Safety Check configuration of Video Port. This structure is used as an argument to IOCTL_DSS_DCTRL_SET_VP_SAFETY_CHK_PARAMS.

Data Fields

uint32_t vpId
 
uint32_t safetySignSeedVal
 
Dss_DctrlRegionSafetyChkCfg regionSafetyChkCfg
 
Dss_DctrlSafetyErrCbFxn safetyErrCbFxn
 
Dss_DctrlVpSafetyCbData safetyCbData
 
void * appData
 

Field Documentation

◆ vpId

uint32_t Dss_DctrlVpSafetyChkParams::vpId

Video Port Id. See CSL_DssVpId for values

◆ safetySignSeedVal

uint32_t Dss_DctrlVpSafetyChkParams::safetySignSeedVal

Safety Signature Seed Value, only one non-zero value is possible in a particular context. In case user passes multiple non-zero values for different regions, previous value is overwritten.

◆ regionSafetyChkCfg

Dss_DctrlRegionSafetyChkCfg Dss_DctrlVpSafetyChkParams::regionSafetyChkCfg

Safety Check Configuration for a particular region. See Dss_DctrlRegionSafetyChkCfg for details

◆ safetyErrCbFxn

Dss_DctrlSafetyErrCbFxn Dss_DctrlVpSafetyChkParams::safetyErrCbFxn

Safety Error callback function

◆ safetyCbData

Dss_DctrlVpSafetyCbData Dss_DctrlVpSafetyChkParams::safetyCbData

Safety Error callback data to be returned to application

◆ appData

void* Dss_DctrlVpSafetyChkParams::appData

Private data of application