AM62x MCU+ SDK  12.00.00
DDR_EccRegion Struct Reference

Detailed Description

DDR Inline ECC region The structure specifies the DDR inline ECC region start and End address.

Data Fields

uint64_t ddrEccStart0
 
uint64_t ddrEccEnd0
 
uint64_t ddrEccPrimeEnd0
 
uint64_t ddrEccStart1
 
uint64_t ddrEccEnd1
 
uint64_t ddrEccPrimeEnd1
 
uint64_t ddrEccStart2
 
uint64_t ddrEccEnd2
 
uint64_t ddrEccPrimeEnd2
 

Field Documentation

◆ ddrEccStart0

uint64_t DDR_EccRegion::ddrEccStart0

DDR inline ECC region-0 start address

◆ ddrEccEnd0

uint64_t DDR_EccRegion::ddrEccEnd0

DDR inline ECC region-0 end address

◆ ddrEccPrimeEnd0

uint64_t DDR_EccRegion::ddrEccPrimeEnd0

DDR inline ECC region-0 primed end address

◆ ddrEccStart1

uint64_t DDR_EccRegion::ddrEccStart1

DDR inline ECC region-1 start address

◆ ddrEccEnd1

uint64_t DDR_EccRegion::ddrEccEnd1

DDR inline ECC region-1 end address

◆ ddrEccPrimeEnd1

uint64_t DDR_EccRegion::ddrEccPrimeEnd1

DDR inline ECC region-1 primed end address

◆ ddrEccStart2

uint64_t DDR_EccRegion::ddrEccStart2

DDR inline ECC region-2 start address

◆ ddrEccEnd2

uint64_t DDR_EccRegion::ddrEccEnd2

DDR inline ECC region-2 end address

◆ ddrEccPrimeEnd2

uint64_t DDR_EccRegion::ddrEccPrimeEnd2

DDR inline ECC region-2 primed end address