AM62x MCU+ SDK  12.00.00

Detailed Description

Data Fields

CpswAle_PolicerMatchParams policerMatch
 
bool threadIdEn
 
uint32_t threadId
 
uint32_t peakRateInBitsPerSec
 
uint32_t commitRateInBitsPerSec
 
CpswAle_PolicerPartLevel policerPartLevel
 

Field Documentation

◆ policerMatch

CpswAle_PolicerMatchParams CpswAle_SetPolicerEntryInPartitionInArgs::policerMatch

Policer match config

◆ threadIdEn

bool CpswAle_SetPolicerEntryInPartitionInArgs::threadIdEn

Enable threadid setting for this policer entry

◆ threadId

uint32_t CpswAle_SetPolicerEntryInPartitionInArgs::threadId

Thread Id which will be enabled for this policer match

◆ peakRateInBitsPerSec

uint32_t CpswAle_SetPolicerEntryInPartitionInArgs::peakRateInBitsPerSec

Peak rate in bits per second. 0 indicates rate limit is disabled

◆ commitRateInBitsPerSec

uint32_t CpswAle_SetPolicerEntryInPartitionInArgs::commitRateInBitsPerSec

Commit rate in bits per second. 0 indicates rate limit is disabled

◆ policerPartLevel

CpswAle_PolicerPartLevel CpswAle_SetPolicerEntryInPartitionInArgs::policerPartLevel

Priority of the entry in policer table