AM62x MCU+ SDK  12.00.00

Detailed Description

DSS Video Pipe DMA related Config parameters.

Data Fields

uint32_t bufPreloadControl
 
uint32_t preloadVal
 
uint32_t bufLowThreshold
 
uint32_t bufHighThreshold
 
uint32_t selfRefreshControl
 
uint32_t selfRefreshEnable
 
uint32_t arbitration
 

Field Documentation

◆ bufPreloadControl

uint32_t CSL_DssVidPipeDmaCfg::bufPreloadControl

Buffer Preload Value can be either pre fixed(set by HW) or as programmed by SW. For valid values see CSL_DssVidPipePreloadControl

◆ preloadVal

uint32_t CSL_DssVidPipeDmaCfg::preloadVal

Buffer Preload Value when preload is SW controlled

◆ bufLowThreshold

uint32_t CSL_DssVidPipeDmaCfg::bufLowThreshold

DMA buffer low threshold. Number of 128 bits defining the threshold value

◆ bufHighThreshold

uint32_t CSL_DssVidPipeDmaCfg::bufHighThreshold

Video DMA buffer high threshold. Number of 128 bits defining the Threshold value

◆ selfRefreshControl

uint32_t CSL_DssVidPipeDmaCfg::selfRefreshControl

Self Refresh transition from disabled to enabled can be controlled by either SW or HW. For valid values see CSL_DssVidPipeRefreshControl

◆ selfRefreshEnable

uint32_t CSL_DssVidPipeDmaCfg::selfRefreshEnable

Enable the self refresh of the video window from its own DMA buffer FALSE: Disable self refresh TRUE: Enable self refresh

◆ arbitration

uint32_t CSL_DssVidPipeDmaCfg::arbitration

Determines the priority of the video pipeline. For valid values see CSL_DssVidPipePriorityVal