Functions | |
int32_t | SafetyCheckers_tifsReqFwlOpen (void) |
API to request TIFS to open firewall. More... | |
int32_t | SafetyCheckers_tifsGetFwlCfg (SafetyCheckers_TifsFwlConfig *fwlConfig, uint32_t size) |
API uses the pointer to firewall configuration fwlConfig as input and updates fwlConfig with the register dump of the firewall registers specified. More... | |
int32_t | SafetyCheckers_tifsVerifyFwlCfg (const SafetyCheckers_TifsFwlConfig *fwlConfig, uint32_t size) |
API compares the fwlConfig (golden reference) with runtime firewall register values and return success or failure. More... | |
int32_t | SafetyCheckers_tifsReqFwlClose (void) |
API to request TIFS to close firewall. More... | |
int32_t SafetyCheckers_tifsReqFwlOpen | ( | void | ) |
API to request TIFS to open firewall.
int32_t SafetyCheckers_tifsGetFwlCfg | ( | SafetyCheckers_TifsFwlConfig * | fwlConfig, |
uint32_t | size | ||
) |
API uses the pointer to firewall configuration fwlConfig as input and updates fwlConfig with the register dump of the firewall registers specified.
fwlConfig | [IN/OUT] Pointer to static firewall configuration to be populated with register values |
size | [IN] Number of entries in the static firewall configuration |
int32_t SafetyCheckers_tifsVerifyFwlCfg | ( | const SafetyCheckers_TifsFwlConfig * | fwlConfig, |
uint32_t | size | ||
) |
API compares the fwlConfig (golden reference) with runtime firewall register values and return success or failure.
fwlConfig | [IN/OUT] Pointer to static firewall configuration / Golden Reference to be verified against |
size | [IN] Number of entries in the static firewall configuration |
int32_t SafetyCheckers_tifsReqFwlClose | ( | void | ) |
API to request TIFS to close firewall.