AM62x MCU+ SDK  12.00.00

Introduction

Sub Modules

 CPSW Statistics
 
 ICSSG Statistics
 

Enumerations

enum  EnetStats_Ioctl {
  ENET_STATS_IOCTL_GET_VERSION = ENET_STATS_PUBLIC_IOCTL(0U), ENET_STATS_IOCTL_PRINT_REGS = ENET_STATS_PUBLIC_IOCTL(1U), ENET_STATS_IOCTL_GET_HOSTPORT_STATS = ENET_STATS_PUBLIC_IOCTL(2U), ENET_STATS_IOCTL_GET_MACPORT_STATS = ENET_STATS_PUBLIC_IOCTL(3U),
  ENET_STATS_IOCTL_RESET_HOSTPORT_STATS = ENET_STATS_PUBLIC_IOCTL(4U), ENET_STATS_IOCTL_RESET_MACPORT_STATS = ENET_STATS_PUBLIC_IOCTL(5U)
}
 Statistics IOCTL commands. More...
 

Macros

#define ENET_STATS_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for STATS module. More...
 

Macro Definition Documentation

◆ ENET_STATS_PUBLIC_IOCTL

#define ENET_STATS_PUBLIC_IOCTL (   x)
Value:
ENET_IOCTL_STATS_BASE | \
ENET_IOCTL_MIN(x))

Helper macro to create IOCTL commands for STATS module.

Enumeration Type Documentation

◆ EnetStats_Ioctl

Statistics IOCTL commands.

Enumerator
ENET_STATS_IOCTL_GET_VERSION 

Get the hardware version of the Stats module.

IOCTL parameters:

ENET_STATS_IOCTL_PRINT_REGS 

Print Stats registers.

IOCTL parameters:

  • inArgs: None
  • outArgs: None
ENET_STATS_IOCTL_GET_HOSTPORT_STATS 

Get host port statistics.

Gets the network statistics of the host port. It's caller's responsibility to typecast the returned statistics structure according to the underlying peripheral's definition.

Use this IOCTL if the statistics module doesn't support separate host port and MAC port statistics.

IOCTL parameters:

  • inArgs: None
  • outArgs: Peripheral/module specific definition.
ENET_STATS_IOCTL_GET_MACPORT_STATS 

Get MAC port statistics.

Gets the network statistics of the given MAC port number. It's caller's responsibility to typecast the returned statistics structure according to the underlying peripheral's definition. For ICSSG MAC mode usecase, port number can't be other than ENET_MAC_PORT_1, as each ICSSG MAC supports only one MAC port.

IOCTL parameters:

  • inArgs: Enet_MacPort
  • outArgs: Peripheral/module specific definition.
ENET_STATS_IOCTL_RESET_HOSTPORT_STATS 

Reset host port statistics.

Resets the network statistics counters of the host port.

Use this IOCTL if the statistics module doesn't support separate host port and MAC port statistics.

IOCTL parameters:

  • inArgs: None
  • outArgs: None
ENET_STATS_IOCTL_RESET_MACPORT_STATS 

Reset MAC port statistics.

Resets the network statistics counters of the given MAC port number. For ICSSG MAC mode usecase, port number can't be other than ENET_MAC_PORT_1, as each ICSSG MAC supports only one MAC port.

IOCTL parameters:

ENET_IOCTL_TYPE_PUBLIC
@ ENET_IOCTL_TYPE_PUBLIC
Definition: enet_ioctl.h:216