This is UDMA driver channel related configuration parameters and API
Files | |
file | udma_ch.h |
UDMA Channel related parameters and API. | |
Data Structures | |
struct | Udma_ChPrms |
UDMA channel open parameters. More... | |
struct | Udma_ChTxPrms |
UDMA TX channel parameters. More... | |
struct | Udma_ChRxPrms |
UDMA RX channel parameters. More... | |
struct | Udma_ChPdmaPrms |
UDMA PDMA channel Static TR parameters. More... | |
struct | Udma_ChStats |
UDMA channel statistics. More... | |
struct | Udma_ChObject |
Opaque UDMA channel object. More... | |
Functions | |
int32_t | Udma_chOpen (Udma_DrvHandle drvHandle, Udma_ChHandle chHandle, uint32_t chType, const Udma_ChPrms *chPrms) |
UDMA open channel. More... | |
int32_t | Udma_chClose (Udma_ChHandle chHandle) |
UDMA close channel. More... | |
int32_t | Udma_chConfigTx (Udma_ChHandle chHandle, const Udma_ChTxPrms *txPrms) |
UDMA configure TX channel. More... | |
int32_t | Udma_chConfigRx (Udma_ChHandle chHandle, const Udma_ChRxPrms *rxPrms) |
UDMA configure RX channel. More... | |
int32_t | Udma_chConfigPdma (Udma_ChHandle chHandle, const Udma_ChPdmaPrms *pdmaPrms) |
UDMA configure PDMA channel (peerChNum as part of Udma_ChPrms) paired with the UDMAP channel. More... | |
int32_t | Udma_chEnable (Udma_ChHandle chHandle) |
UDMA channel enable API. More... | |
int32_t | Udma_chDisable (Udma_ChHandle chHandle, uint32_t timeout) |
UDMA channel teardown and disable API. More... | |
int32_t | Udma_chPause (Udma_ChHandle chHandle) |
UDMA channel pause API. More... | |
int32_t | Udma_chResume (Udma_ChHandle chHandle) |
UDMA channel resume API. More... | |
uint32_t | Udma_chGetNum (Udma_ChHandle chHandle) |
Returns the channel number offset with in a channel type - TX, RX and External (UTC) channel types. More... | |
Udma_RingHandle | Udma_chGetFqRingHandle (Udma_ChHandle chHandle) |
Returns the default free ring handle of the channel. More... | |
Udma_RingHandle | Udma_chGetCqRingHandle (Udma_ChHandle chHandle) |
Returns the default completion ring handle of the channel. More... | |
Udma_RingHandle | Udma_chGetTdCqRingHandle (Udma_ChHandle chHandle) |
Returns the teardown completion ring handle of the channel. More... | |
uint16_t | Udma_chGetFqRingNum (Udma_ChHandle chHandle) |
Returns the default free ring number to be programmed in descriptor. More... | |
uint16_t | Udma_chGetCqRingNum (Udma_ChHandle chHandle) |
Returns the default completion ring number to be programmed in descriptor. More... | |
Udma_FlowHandle | Udma_chGetDefaultFlowHandle (Udma_ChHandle chHandle) |
Returns the default flow handle of the RX channel. More... | |
uint32_t | Udma_chGetTriggerEvent (Udma_ChHandle chHandle, uint32_t trigger) |
Returns the global trigger event for the channel. More... | |
void * | Udma_chGetSwTriggerRegister (Udma_ChHandle chHandle) |
Returns the software trigger register address for the channel. More... | |
int32_t | Udma_chSetSwTrigger (Udma_ChHandle chHandle, uint32_t trigger) |
Sets the software trigger register based on the trigger mode provided. More... | |
int32_t | Udma_chSetChaining (Udma_ChHandle triggerChHandle, Udma_ChHandle chainedChHandle, uint32_t trigger) |
Chains the trigger channel with the chained channel. More... | |
int32_t | Udma_chBreakChaining (Udma_ChHandle triggerChHandle, Udma_ChHandle chainedChHandle) |
Breaks the chaining by resetting the trigger channel's OES. More... | |
void | UdmaChPrms_init (Udma_ChPrms *chPrms, uint32_t chType) |
Udma_ChPrms structure init function. More... | |
void | UdmaChTxPrms_init (Udma_ChTxPrms *txPrms, uint32_t chType) |
Udma_ChTxPrms structure init function. More... | |
void | UdmaChRxPrms_init (Udma_ChRxPrms *rxPrms, uint32_t chType) |
Udma_ChRxPrms structure init function. More... | |
void | UdmaChPdmaPrms_init (Udma_ChPdmaPrms *pdmaPrms) |
Udma_ChPdmaPrms structure init function. More... | |
int32_t | Udma_chGetStats (Udma_ChHandle chHandle, Udma_ChStats *chStats) |
Get real-time channel statistics. More... | |
int32_t | Udma_getPeerData (Udma_ChHandle chHandle, uint32_t *peerData) |
Get real-time peer data which contains number of bytes written. More... | |
int32_t | Udma_clearPeerData (Udma_ChHandle chHandle, uint32_t peerData) |
Clear real-time peer data which contains number of bytes written. More... | |
int32_t | Udma_chReset (Udma_ChHandle chHandle) |
Hard reset the channel if teardown fails. More... | |
Macros | |
#define | UDMA_DMA_CH_INVALID ((uint32_t) 0xFFFF0000U) |
Macro used to specify that DMA Channel ID is invalid. Used in the API Udma_chOpen. More... | |
#define | UDMA_DMA_CH_ANY ((uint32_t) 0xFFFF0001U) |
Macro used to specify any available DMA Channel while requesting one. Used in the API Udma_chOpen. More... | |
#define | UDMA_DMA_CH_NA ((uint32_t) 0xFFFF0002U) |
Macro used to specify that the DMA Channel is not applicable for a particular mode. More... | |
#define | UDMA_MAPPED_GROUP_INVALID ((uint32_t) 0xFFFF0004U) |
Macro used to specify that the Mapped Channel Group is invalid. More... | |
#define | UDMA_SYSFW_EXTENDED_CH_TYPE_BCDMA_BLK_CPY ((uint8_t) 1U) |
SYSFW Extended Channel Type Flag for BCDMA Block Copy. More... | |
#define | UDMA_SYSFW_EXTENDED_CH_TYPE_BCDMA_SPLIT_TR_TX ((uint8_t) 0U) |
SYSFW Extended Channel Type Flag for BCDMA split TR TX channels. More... | |
UDMA Channel Flag | |
UDMA channel flags bit field used to form the channel type. | |
#define | UDMA_CH_FLAG_TX ((uint32_t) 0x0001U) |
TX channel flag. More... | |
#define | UDMA_CH_FLAG_RX ((uint32_t) 0x0002U) |
RX channel flag. More... | |
#define | UDMA_CH_FLAG_BLK_COPY ((uint32_t) 0x0004U) |
Block copy mode channel flag. More... | |
#define | UDMA_CH_FLAG_PDMA ((uint32_t) 0x0008U) |
PDMA channel flag. More... | |
#define | UDMA_CH_FLAG_PSIL ((uint32_t) 0x0010U) |
PSIL channel flag meant for periperals like Ethernet, SA2UL. More... | |
#define | UDMA_CH_FLAG_HC ((uint32_t) 0x0040U) |
High capacity channel flag. More... | |
#define | UDMA_CH_FLAG_UHC ((uint32_t) 0x0080U) |
Ultra high capacity channel flag. More... | |
#define | UDMA_CH_FLAG_MAPPED ((uint32_t) 0x0100U) |
Mapped TX/RX channel flag. More... | |
UDMA PDMA element size | |
#define | UDMA_PDMA_ES_8BITS ((uint32_t) 0x00U) |
#define | UDMA_PDMA_ES_16BITS ((uint32_t) 0x01U) |
#define | UDMA_PDMA_ES_24BITS ((uint32_t) 0x02U) |
#define | UDMA_PDMA_ES_32BITS ((uint32_t) 0x03U) |
#define | UDMA_PDMA_ES_64BITS ((uint32_t) 0x04U) |
#define | UDMA_PDMA_ES_DONTCARE ((uint32_t) 0x00U) |
Set this for MCAN element size - not applicable. More... | |
#define UDMA_DMA_CH_INVALID ((uint32_t) 0xFFFF0000U) |
Macro used to specify that DMA Channel ID is invalid. Used in the API Udma_chOpen.
#define UDMA_DMA_CH_ANY ((uint32_t) 0xFFFF0001U) |
Macro used to specify any available DMA Channel while requesting one. Used in the API Udma_chOpen.
#define UDMA_DMA_CH_NA ((uint32_t) 0xFFFF0002U) |
Macro used to specify that the DMA Channel is not applicable for a particular mode.
#define UDMA_MAPPED_GROUP_INVALID ((uint32_t) 0xFFFF0004U) |
Macro used to specify that the Mapped Channel Group is invalid.
#define UDMA_SYSFW_EXTENDED_CH_TYPE_BCDMA_BLK_CPY ((uint8_t) 1U) |
SYSFW Extended Channel Type Flag for BCDMA Block Copy.
#define UDMA_SYSFW_EXTENDED_CH_TYPE_BCDMA_SPLIT_TR_TX ((uint8_t) 0U) |
SYSFW Extended Channel Type Flag for BCDMA split TR TX channels.
#define UDMA_CH_FLAG_TX ((uint32_t) 0x0001U) |
TX channel flag.
#define UDMA_CH_FLAG_RX ((uint32_t) 0x0002U) |
RX channel flag.
#define UDMA_CH_FLAG_BLK_COPY ((uint32_t) 0x0004U) |
Block copy mode channel flag.
#define UDMA_CH_FLAG_PDMA ((uint32_t) 0x0008U) |
PDMA channel flag.
#define UDMA_CH_FLAG_PSIL ((uint32_t) 0x0010U) |
PSIL channel flag meant for periperals like Ethernet, SA2UL.
#define UDMA_CH_FLAG_HC ((uint32_t) 0x0040U) |
High capacity channel flag.
#define UDMA_CH_FLAG_UHC ((uint32_t) 0x0080U) |
Ultra high capacity channel flag.
#define UDMA_CH_FLAG_MAPPED ((uint32_t) 0x0100U) |
Mapped TX/RX channel flag.
#define UDMA_CH_TYPE_TR_BLK_COPY |
TR block copy type - TX/RX pair.
#define UDMA_CH_TYPE_TR_BLK_COPY_HC |
High capacity TR block copy type - TX/RX pair.
#define UDMA_CH_TYPE_TR_BLK_COPY_UHC |
Ultra high capacity TR block copy type - TX/RX pair.
#define UDMA_CH_TYPE_TX (UDMA_CH_FLAG_TX | UDMA_CH_FLAG_PSIL) |
TX channel type.
#define UDMA_CH_TYPE_TX_HC (UDMA_CH_FLAG_TX | UDMA_CH_FLAG_PSIL | UDMA_CH_FLAG_HC) |
High capacity TX channel type.
#define UDMA_CH_TYPE_TX_UHC (UDMA_CH_FLAG_TX | UDMA_CH_FLAG_PSIL | UDMA_CH_FLAG_UHC) |
Ultra high capacity TX channel type.
#define UDMA_CH_TYPE_RX (UDMA_CH_FLAG_RX | UDMA_CH_FLAG_PSIL) |
RX channel type.
#define UDMA_CH_TYPE_RX_HC (UDMA_CH_FLAG_RX | UDMA_CH_FLAG_PSIL | UDMA_CH_FLAG_HC) |
High capacity RX channel type.
#define UDMA_CH_TYPE_RX_UHC (UDMA_CH_FLAG_RX | UDMA_CH_FLAG_PSIL | UDMA_CH_FLAG_UHC) |
Ultra high capacity RX channel type.
#define UDMA_CH_TYPE_PDMA_TX (UDMA_CH_FLAG_TX | UDMA_CH_FLAG_PDMA) |
PDMA TX channel type.
#define UDMA_CH_TYPE_PDMA_TX_HC (UDMA_CH_FLAG_TX | UDMA_CH_FLAG_PDMA | UDMA_CH_FLAG_HC) |
High capacity PDMA TX channel type.
#define UDMA_CH_TYPE_PDMA_TX_UHC (UDMA_CH_FLAG_TX | UDMA_CH_FLAG_PDMA | UDMA_CH_FLAG_UHC) |
Ultra high capacity PDMA TX channel type.
#define UDMA_CH_TYPE_PDMA_RX (UDMA_CH_FLAG_RX | UDMA_CH_FLAG_PDMA) |
PDMA RX channel type.
#define UDMA_CH_TYPE_PDMA_RX_HC (UDMA_CH_FLAG_RX | UDMA_CH_FLAG_PDMA | UDMA_CH_FLAG_HC) |
High capacity PDMA RX channel type.
#define UDMA_CH_TYPE_PDMA_RX_UHC (UDMA_CH_FLAG_RX | UDMA_CH_FLAG_PDMA | UDMA_CH_FLAG_UHC) |
Ultra high capacity PDMA RX channel type.
#define UDMA_CH_TYPE_TX_MAPPED (UDMA_CH_FLAG_TX | UDMA_CH_FLAG_PSIL | UDMA_CH_FLAG_MAPPED) |
Mapped TX channel. This could be different type of mapped TX channels. See Udma_MappedTxGrpSoc for differnt types of SOC specific mapped TX channels.
#define UDMA_CH_TYPE_RX_MAPPED (UDMA_CH_FLAG_RX | UDMA_CH_FLAG_PSIL | UDMA_CH_FLAG_MAPPED) |
Mapped RX channel. This could be different type of mapped RX channels. See Udma_MappedRxGrpSoc for differnt types of SOC specific mapped RX channels.
#define UDMA_PDMA_ES_8BITS ((uint32_t) 0x00U) |
#define UDMA_PDMA_ES_16BITS ((uint32_t) 0x01U) |
#define UDMA_PDMA_ES_24BITS ((uint32_t) 0x02U) |
#define UDMA_PDMA_ES_32BITS ((uint32_t) 0x03U) |
#define UDMA_PDMA_ES_64BITS ((uint32_t) 0x04U) |
#define UDMA_PDMA_ES_DONTCARE ((uint32_t) 0x00U) |
Set this for MCAN element size - not applicable.
int32_t Udma_chOpen | ( | Udma_DrvHandle | drvHandle, |
Udma_ChHandle | chHandle, | ||
uint32_t | chType, | ||
const Udma_ChPrms * | chPrms | ||
) |
UDMA open channel.
Opens the UDMA channel based on the channel parameters. This also does the PSILCFG pairing based on the peer thread ID provided.
Requirement: DOX_REQ_TAG(PDK-2578)
drvHandle | [IN] UDMA driver handle pointer passed during Udma_init |
chHandle | [IN/OUT] UDMA channel handle. The caller need to allocate memory for this object and pass this pointer to all further APIs. The caller should not change any parameters as this is owned and maintained by the driver. This parameter can't be NULL. |
chType | [IN] UDMA channel type. Refer Udma_ChType. |
chPrms | [IN] UDMA channel parameters. This parameter can't be NULL. |
int32_t Udma_chClose | ( | Udma_ChHandle | chHandle | ) |
UDMA close channel.
Closes the UDMA channel and frees all associated resources.
Requirement: DOX_REQ_TAG(PDK-2579)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
int32_t Udma_chConfigTx | ( | Udma_ChHandle | chHandle, |
const Udma_ChTxPrms * | txPrms | ||
) |
UDMA configure TX channel.
Configures the TX channel parameters. Note: This is applicable only when the channel type is TX
Note: This API can't be called after channel enable.
Requirement: DOX_REQ_TAG(PDK-2580)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
txPrms | [IN] UDMA TX channel parameter. Refer Udma_ChTxPrms. |
int32_t Udma_chConfigRx | ( | Udma_ChHandle | chHandle, |
const Udma_ChRxPrms * | rxPrms | ||
) |
UDMA configure RX channel.
Configures the RX channel parameters. Note: This is applicable only when the channel type is RX In case of BCDMA Block Copy, there is no need to configure RX Channel. Therfore the function returns gracefully, without doing anything.
Note: This API can't be called after channel enable.
Requirement: DOX_REQ_TAG(PDK-2581)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
rxPrms | [IN] UDMA RX channel parameter. Refer Udma_ChRxPrms. |
int32_t Udma_chConfigPdma | ( | Udma_ChHandle | chHandle, |
const Udma_ChPdmaPrms * | pdmaPrms | ||
) |
UDMA configure PDMA channel (peerChNum as part of Udma_ChPrms) paired with the UDMAP channel.
This configures the PDMA channel static X,Y,Z parameters.
Requirement: DOX_REQ_TAG(PDK-2583)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
pdmaPrms | [IN] UDMA RX channel parameter. Refer Udma_ChPdmaPrms. |
int32_t Udma_chEnable | ( | Udma_ChHandle | chHandle | ) |
UDMA channel enable API.
This function will enable the UDMA channel.
Requirement: DOX_REQ_TAG(PDK-2584)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
int32_t Udma_chDisable | ( | Udma_ChHandle | chHandle, |
uint32_t | timeout | ||
) |
UDMA channel teardown and disable API.
This function will perform the channel teardown and eventually disables the UDMA channel. This initiates the force teardown sequence based on the channel type and wait for teardown to complete gracefully. If the teardown doesn't complete within the timeout provided, then this will initiate a force teardown sequence.
Caution: This API is blocking. Hence cannot be called from ISR context!!
Requirement: DOX_REQ_TAG(PDK-2585)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
timeout | [IN] Timeout in ms. Use SystemP_WAIT_FOREVER to wait forever. |
int32_t Udma_chPause | ( | Udma_ChHandle | chHandle | ) |
UDMA channel pause API.
This function will pause the UDMA channel by setting the pause bit of the UDMAP runtime register.
Requirement: DOX_REQ_TAG(PDK-2977)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
int32_t Udma_chResume | ( | Udma_ChHandle | chHandle | ) |
UDMA channel resume API.
This function will resume the UDMA channel by clearing the pause bit of the UDMAP runtime register.
Requirement: DOX_REQ_TAG(PDK-2977)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
uint32_t Udma_chGetNum | ( | Udma_ChHandle | chHandle | ) |
Returns the channel number offset with in a channel type - TX, RX and External (UTC) channel types.
In case of UTC type, this returns the relative offset from the start of UTC it belongs to (and not from the external channel start).
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
Udma_RingHandle Udma_chGetFqRingHandle | ( | Udma_ChHandle | chHandle | ) |
Returns the default free ring handle of the channel.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
Udma_RingHandle Udma_chGetCqRingHandle | ( | Udma_ChHandle | chHandle | ) |
Returns the default completion ring handle of the channel.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
Udma_RingHandle Udma_chGetTdCqRingHandle | ( | Udma_ChHandle | chHandle | ) |
Returns the teardown completion ring handle of the channel.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
uint16_t Udma_chGetFqRingNum | ( | Udma_ChHandle | chHandle | ) |
Returns the default free ring number to be programmed in descriptor.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
uint16_t Udma_chGetCqRingNum | ( | Udma_ChHandle | chHandle | ) |
Returns the default completion ring number to be programmed in descriptor.
Requirement: DOX_REQ_TAG(PDK-2586)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
Udma_FlowHandle Udma_chGetDefaultFlowHandle | ( | Udma_ChHandle | chHandle | ) |
Returns the default flow handle of the RX channel.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
uint32_t Udma_chGetTriggerEvent | ( | Udma_ChHandle | chHandle, |
uint32_t | trigger | ||
) |
Returns the global trigger event for the channel.
This function will return the appropriate global 0/1 trigger event for the channel.
Notes: Trigger is not supported for external channels and the function will return UDMA_EVENT_INVALID.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
trigger | [IN] Global0 or Global 1 Trigger - refer CSL_UdmapTrFlagsTrigger |
void* Udma_chGetSwTriggerRegister | ( | Udma_ChHandle | chHandle | ) |
Returns the software trigger register address for the channel.
This function will return the appropriate SW trigger register. Incase of UDMAP channels, it returns the 32-bit TX SWTRIG register address. Incase of DRU channels, it returns the 64-bit DRU CHRT_SWTRIG register address.
Notes: SW trigger is not supported for RX channels. Incase of TX channels, only global trigger 0 is supported. Incase of DRU channels, global trigger 0/1 and local events are supported.
Requirement: DOX_REQ_TAG(PDK-2594)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
int32_t Udma_chSetSwTrigger | ( | Udma_ChHandle | chHandle, |
uint32_t | trigger | ||
) |
Sets the software trigger register based on the trigger mode provided.
This function will set the appropriate SW trigger register. Incase of UDMAP channels, it will set in the TX SWTRIG register. Incase of DRU channels, it will set in the DRU CHRT_SWTRIG register.
Notes: SW trigger is not supported for RX channels. Incase of TX channels, only global trigger 0 is supported. Incase of DRU channels, global trigger 0/1 and local events are supported.
Requirement: DOX_REQ_TAG(PDK-2594)
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
trigger | [IN] Global0 or Global 1 Trigger - refer CSL_UdmapTrFlagsTrigger |
int32_t Udma_chSetChaining | ( | Udma_ChHandle | triggerChHandle, |
Udma_ChHandle | chainedChHandle, | ||
uint32_t | trigger | ||
) |
Chains the trigger channel with the chained channel.
This programs the trigger channel TR event register (OES) to the global trigger (0 or 1) event of the chained channel.
Once this is done, the application should set the TR trigger (0 or 1) of the trigger channel while submitting TR to the trigger channel. Based on the trigger type (full, ICNT0, INCT1, ICNT3), the trigger channel will trigger the "chained" channel through the channel OES.
Note: Only global0 and global1 triggers are supported.
triggerChHandle | [IN] UDMA channel handle which triggers the chain. This parameter can't be NULL. |
chainedChHandle | [IN] UDMA channel handle which gets triggered. This parameter can't be NULL. |
trigger | [IN] Global0 or Global 1 Trigger - refer CSL_UdmapTrFlagsTrigger |
int32_t Udma_chBreakChaining | ( | Udma_ChHandle | triggerChHandle, |
Udma_ChHandle | chainedChHandle | ||
) |
Breaks the chaining by resetting the trigger channel's OES.
Note: Only global0 and global1 triggers are supported.
triggerChHandle | [IN] UDMA channel handle which triggers the chain. This parameter can't be NULL. |
chainedChHandle | [IN] UDMA channel handle which gets triggered. This parameter can't be NULL. |
void UdmaChPrms_init | ( | Udma_ChPrms * | chPrms, |
uint32_t | chType | ||
) |
Udma_ChPrms structure init function.
chPrms | [IN] Pointer to Udma_ChPrms structure. |
chType | [IN] UDMA channel type. Refer Udma_ChType. |
void UdmaChTxPrms_init | ( | Udma_ChTxPrms * | txPrms, |
uint32_t | chType | ||
) |
Udma_ChTxPrms structure init function.
txPrms | [IN] Pointer to Udma_ChTxPrms structure. |
chType | [IN] UDMA channel type. Refer Udma_ChType. |
void UdmaChRxPrms_init | ( | Udma_ChRxPrms * | rxPrms, |
uint32_t | chType | ||
) |
Udma_ChRxPrms structure init function.
rxPrms | [IN] Pointer to Udma_ChRxPrms structure. |
chType | [IN] UDMA channel type. Refer Udma_ChType. |
void UdmaChPdmaPrms_init | ( | Udma_ChPdmaPrms * | pdmaPrms | ) |
Udma_ChPdmaPrms structure init function.
pdmaPrms | [IN] Pointer to Udma_ChPdmaPrms structure. |
int32_t Udma_chGetStats | ( | Udma_ChHandle | chHandle, |
Udma_ChStats * | chStats | ||
) |
Get real-time channel statistics.
Requirement: PRSDK-5609
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
chStats | [IN] Pointer to Udma_ChStats. This parameter can't be NULL. |
int32_t Udma_getPeerData | ( | Udma_ChHandle | chHandle, |
uint32_t * | peerData | ||
) |
Get real-time peer data which contains number of bytes written.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
peerData | [INOUT] Pointer to peer data. |
int32_t Udma_clearPeerData | ( | Udma_ChHandle | chHandle, |
uint32_t | peerData | ||
) |
Clear real-time peer data which contains number of bytes written.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |
peerData | [IN] Peer data. |
int32_t Udma_chReset | ( | Udma_ChHandle | chHandle | ) |
Hard reset the channel if teardown fails.
chHandle | [IN] UDMA channel handle. This parameter can't be NULL. |