AM62x MCU+ SDK  12.00.00
dp83826.h File Reference

Introduction

This file contains the type definitions and helper macros for the DP83826 Ethernet PHY.

Go to the source code of this file.

Data Structures

struct  Dp83826_Cfg
 dp83826 PHY configuration parameters. More...
 

Functions

void Dp83826_initCfg (Dp83826_Cfg *cfg)
 Initialize dp83826 PHY specific config params. More...
 
void Dp83826_bind (EthPhyDrv_Handle *hPhy, uint8_t phyAddr, Phy_RegAccessCb_t *pRegAccessCb)
 
bool Dp83826_isPhyDevSupported (EthPhyDrv_Handle hPhy, const void *pVersion)
 
bool Dp83826_isMacModeSupported (EthPhyDrv_Handle hPhy, Phy_Mii mii)
 
int32_t Dp83826_config (EthPhyDrv_Handle hPhy, const void *pExtCfg, const uint32_t extCfgSize, Phy_Mii mii, bool loopbackEn)
 
void Dp83826_printRegs (EthPhyDrv_Handle hPhy)