AM62x MCU+ SDK  12.00.00
HwiP.h File Reference

Go to the source code of this file.

Data Structures

struct  HwiP_Config
 HwiP config parameters, setup as part of SysConfig, not to be set by end-users directly. More...
 
struct  HwiP_Params
 Parameters passed during HwiP_construct. More...
 
struct  HwiP_Object
 Opaque Hwi object used with the Hwi APIs. More...
 
struct  AIFSR
 Provide additional information about data and instruction parity, ECC, and external TCM errors. More...
 
struct  IFSR
 Holds status information regarding the source of the last instruction abort. More...
 
struct  ADFSR
 Provide additional information about data and instruction parity, ECC, and external TCM errors. More...
 
struct  DFSR
 Holds status information regarding the source of the last data abort. More...
 

Macros

#define HWIP_INVALID_EVENT_ID   (0xFFFFU)
 
#define HwiP_OBJECT_SIZE_MAX   (32u)
 Max size of Hwi object across no-RTOS and all OS's. More...
 

Typedefs

typedef void(* HwiP_FxnCallback) (void *args)
 Callback that is called when a HW interrupt is received. More...
 

Functions

void HwiP_Params_init (HwiP_Params *params)
 Set default values to HwiP_Params. More...
 
int32_t HwiP_construct (HwiP_Object *obj, HwiP_Params *params)
 Create a Hwi object. More...
 
int32_t HwiP_setArgs (HwiP_Object *obj, void *args)
 Set argument to pass to the ISR. More...
 
void HwiP_destruct (HwiP_Object *obj)
 Cleanup, delete, destruct a Hwi object. More...
 
void HwiP_enableInt (uint32_t intNum)
 Enable a specific interrupt. More...
 
uint32_t HwiP_disableInt (uint32_t intNum)
 Disable a specific interrupt. More...
 
void HwiP_restoreInt (uint32_t intNum, uint32_t oldIntState)
 Restore a specific interrupt. More...
 
void HwiP_clearInt (uint32_t intNum)
 Clear a pending specific interrupt. More...
 
void HwiP_post (uint32_t intNum)
 Force trigger a specific interrupt. More...
 
uintptr_t HwiP_disable (void)
 Disable all interrupts. More...
 
void HwiP_enable (void)
 Enable all interrupts. More...
 
void HwiP_restore (uintptr_t oldIntState)
 Restores all interrupts to a given state. More...
 
uint32_t HwiP_inISR (void)
 Check if the caller of this function is inside a ISR or not. More...
 
void HwiP_init (void)
 Initialize Hwi module. More...
 
int32_t HwiP_registerNmiHandler (HwiP_FxnCallback nmiHandler, void *args)
 This API registers the NMI handler. More...
 
int32_t HwiP_unregisterNmiHandler (void)
 This API unregisters the current NMI handler. More...
 

Macro Definition Documentation

◆ HWIP_INVALID_EVENT_ID

#define HWIP_INVALID_EVENT_ID   (0xFFFFU)