AM62x MCU+ SDK  12.00.00
Driver Porting Layer (DPL) demo

Introduction

This example shows a simple application, which setups the CPU and the underlying RTOS or no-RTOS environment on the supported SOC.

The example does the below

  • Setup a timer with system tick of 1ms, setup MPU and cache (if available)
  • Create a RTOS task (in RTOS example)
  • Trigger a ISR and signal a semaphore from ISR to main task
  • Show usage of clock delay
  • Show usage of cache APIs
  • Show usage of heap APIs

Supported Combinations

Parameter Value
CPU + OS m4fss0-0 nortos
m4fss0-0 freertos
r5fss0-0 freertos
a53ss0-0 nortos
a53ss0-0 freertos
a53ss0-1 freertos
a53ss0-1 nortos
a53ss1-0 freertos
a53ss1-0 nortos
a53ss1-1 freertos
a53ss1-1 nortos
a53ss0-0 freertos-smp
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am62x-sk, am62x-sk-lp, am62x-sip-sk
Example folder examples/kernel/dpl/dpl_demo/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • To run the example on a53ss0-0, a53ss0-1, a53ss1-0 and a53ss1-1 in FreeRTOS-AMP mode, run the dpl_demo_freertos-amp_sbl_uart_hs_fs.cfg file using SBL UART or load and run through CCS individually

See Also

Driver Porting Layer (DPL)

Sample Output

Shown below is a sample output when the application is run,

[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[DPL] Sleep ... DONE (Measured time = 100000 usecs, CPU cycles = 80000055 ) !!!
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x80010440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x80010440, heap free size = 1984 bytes
All tests have passed!

FreeRTOS-AMP Sample Output

Attention
Output from a53ss0-1, a53ss1-0 and a53ss1-1 cores are log to the Shared memory, can be viewed via a53ss0-0 on which log reader is enabled

Shown below is a sample output on UART0 console when the application is run,

NOTICE: BL31: v2.11.0(release):v2.11.0-906-g58b25570c
NOTICE: BL31: Built : 16:12:49, Dec 16 2024
DPL Demo Example started on a53_core0
[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Hwi(sgi) post ...
[DPL] Hwi(sgi) post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[a530-1] 0.000095s : DPL Demo Example started on a53_core1
[DPL] Hwi post ...109s :
[a530-1] 0.000121s : [DPL] Hwi post ... DONE !!!
[a530-1] 0.000127s : [DPL] Hwi(sgi) post ...
[a530-1] 0.000132s : [DPL] Hwi(sgi) post ... DONE !!!
[a530-1] 0.000135s : [DPL] Sleep for 100 msecs ...
[a531-0] 0.000086s : DPL Demo Example started on a53_core2
[DPL] Hwi post ...100s :
[a531-0] 0.000112s : [DPL] Hwi post ... DONE !!!
[a531-0] 0.000118s : [DPL] Hwi(sgi) post ...
[a531-0] 0.000123s : [DPL] Hwi(sgi) post ... DONE !!!
[a531-0] 0.000126s : [DPL] Sleep for 100 msecs ...
[a531-1] 0.000103s : DPL Demo Example started on a53_core3
[DPL] Hwi post ...116s :
[a531-1] 0.000128s : [DPL] Hwi post ... DONE !!!
[a531-1] 0.000134s : [DPL] Hwi(sgi) post ...
[a531-1] 0.000138s : [DPL] Hwi(sgi) post ... DONE !!!
[a531-1] 0.000141s : [DPL] Sleep for 100 msecs ...
[a531-1] 0.100003s : [DPL] Sleep ... DONE (Measured time = 99859 usecs, CPU cycles = 167570 ) !!!
[a531-1] 0.100008s : Note: In case of FREERTOS CPU Cycles will not match with the measured time
[DPL] Sleep ... DONE (Measured time = 99801 usecs, CPU cycles = 11863381 ) !!!
Note: In case of FREERTOS CPU Cycles will not match with the measured time
As the "WFI" instruction is called from idle task, which suspends the PMU counter used to mea.
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x800a0440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x800a0440, heap free size = 1984 bytes
All tests have passed on a53_core0 !!
[a531-1] 0.100012s : As the "WFI" instruction is called from idle task, which suspends thes
[a531-1] 0.100017s : ure CPU cycles.
[a531-1] 0.100020s : [DPL] Running cache operations ...
[a531-1] 0.100025s : [DPL] Running cache operations ... DONE !!!
[a531-1] 0.100029s : [DPL] Heap free size = 1984 bytes
[a531-1] 0.100034s : [DPL] Allocated 1023 bytes @ 0x88110440, heap free size = 896 bytes
[a531-1] 0.100041s : [DPL] Free'ed 1023 bytes @ 0x88110440, heap free size = 1984 bytes
[a531-1] 0.100046s : All tests have passed on a53_core3 !!
[a530-1] 0.100003s : [DPL] Sleep ... DONE (Measured time = 99865 usecs, CPU cycles = 167076 ) !!!
[a530-1] 0.100009s : Note: In case of FREERTOS CPU Cycles will not match with the measured time
[a530-1] 0.100013s : As the "WFI" instruction is called from idle task, which suspends thes
[a530-1] 0.100017s : ure CPU cycles.
[a530-1] 0.100020s : [DPL] Running cache operations ...
[a530-1] 0.100025s : [DPL] Running cache operations ... DONE !!!
[a530-1] 0.100029s : [DPL] Heap free size = 1984 bytes
[a530-1] 0.100035s : [DPL] Allocated 1023 bytes @ 0x82110440, heap free size = 896 bytes
[a530-1] 0.100041s : [DPL] Free'ed 1023 bytes @ 0x82110440, heap free size = 1984 bytes
[a530-1] 0.100046s : All tests have passed on a53_core1 !!
[a531-0] 0.100003s : [DPL] Sleep ... DONE (Measured time = 99874 usecs, CPU cycles = 166969 ) !!!
[a531-0] 0.100008s : Note: In case of FREERTOS CPU Cycles will not match with the measured time
[a531-0] 0.100012s : As the "WFI" instruction is called from idle task, which suspends thes
[a531-0] 0.100017s : ure CPU cycles.
[a531-0] 0.100020s : [DPL] Running cache operations ...
[a531-0] 0.100025s : [DPL] Running cache operations ... DONE !!!
[a531-0] 0.100029s : [DPL] Heap free size = 1984 bytes
[a531-0] 0.100035s : [DPL] Allocated 1023 bytes @ 0x86090440, heap free size = 896 bytes
[a531-0] 0.100041s : [DPL] Free'ed 1023 bytes @ 0x86090440, heap free size = 1984 bytes
[a531-0] 0.100046s : All tests have passed on a53_core2 !!