This is UDMA driver common parameters and API
|
| file | udma_types.h |
| | UDMA Low Level Driver API/interface data types file.
|
| |
|
Error codes returned by UDMA APIs
|
| #define | UDMA_SOK ( (int32_t) (0)) |
| | API call successful. More...
|
| |
| #define | UDMA_EFAIL (-(int32_t) (1)) |
| | API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure. More...
|
| |
| #define | UDMA_EBADARGS (-(int32_t) (2)) |
| | API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected. More...
|
| |
| #define | UDMA_EINVALID_PARAMS (-(int32_t) (3)) |
| | API call returned with error as invalid parameters. Typically when parameters passed are not valid or out of range. More...
|
| |
| #define | UDMA_ETIMEOUT (-(int32_t) (4)) |
| | API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period. More...
|
| |
| #define | UDMA_EALLOC (-(int32_t) (5)) |
| | API call returned with error as allocation failed. More...
|
| |
◆ UDMA_CACHELINE_ALIGNMENT
| #define UDMA_CACHELINE_ALIGNMENT (128U) |
Cache line size for alignment of descriptor and buffers.
◆ UDMA_ALIGN_SIZE
Macro to align the size in bytes to UDMA cache line alignment.
◆ UDMA_DEFAULT_CH_DISABLE_TIMEOUT
| #define UDMA_DEFAULT_CH_DISABLE_TIMEOUT (100U) |
Default UDMA channel disable timeout.
◆ UDMA_SOK
| #define UDMA_SOK ( (int32_t) (0)) |
◆ UDMA_EFAIL
| #define UDMA_EFAIL (-(int32_t) (1)) |
API call returned with error as failed. Used for generic error. It may be some hardware failure and/or software failure.
◆ UDMA_EBADARGS
| #define UDMA_EBADARGS (-(int32_t) (2)) |
API call returned with error as bad arguments. Typically, NULL pointer passed to the API where its not expected.
◆ UDMA_EINVALID_PARAMS
| #define UDMA_EINVALID_PARAMS (-(int32_t) (3)) |
API call returned with error as invalid parameters. Typically when parameters passed are not valid or out of range.
◆ UDMA_ETIMEOUT
| #define UDMA_ETIMEOUT (-(int32_t) (4)) |
API call returned with error as timed out. Typically API is waiting for some condition and returned as condition not happened in the timeout period.
◆ UDMA_EALLOC
| #define UDMA_EALLOC (-(int32_t) (5)) |
API call returned with error as allocation failed.
◆ UDMA_INST_ID_0
| #define UDMA_INST_ID_0 (0U) |
◆ UDMA_INST_ID_1
| #define UDMA_INST_ID_1 (1U) |
◆ UDMA_INST_ID_2
| #define UDMA_INST_ID_2 (2U) |
◆ UDMA_INST_ID_3
| #define UDMA_INST_ID_3 (3U) |
◆ UDMA_UTC_ID0
| #define UDMA_UTC_ID0 (0U) |
◆ UDMA_UTC_ID1
| #define UDMA_UTC_ID1 (1U) |
◆ UDMA_UTC_ID2
| #define UDMA_UTC_ID2 (2U) |
◆ UDMA_UTC_ID3
| #define UDMA_UTC_ID3 (3U) |
◆ UDMA_UTC_ID4
| #define UDMA_UTC_ID4 (4U) |
◆ UDMA_UTC_ID5
| #define UDMA_UTC_ID5 (5U) |
◆ UDMA_UTC_ID6
| #define UDMA_UTC_ID6 (6U) |
◆ UDMA_UTC_ID7
| #define UDMA_UTC_ID7 (7U) |
◆ UDMA_UTC_ID8
| #define UDMA_UTC_ID8 (8U) |
◆ UDMA_UTC_ID9
| #define UDMA_UTC_ID9 (9U) |
◆ UDMA_MAPPED_GROUP0
| #define UDMA_MAPPED_GROUP0 (0U) |
◆ UDMA_MAPPED_GROUP1
| #define UDMA_MAPPED_GROUP1 (1U) |
◆ UDMA_MAPPED_GROUP2
| #define UDMA_MAPPED_GROUP2 (2U) |
◆ UDMA_MAPPED_GROUP3
| #define UDMA_MAPPED_GROUP3 (3U) |
◆ UDMA_MAPPED_GROUP4
| #define UDMA_MAPPED_GROUP4 (4U) |
◆ UDMA_MAPPED_GROUP5
| #define UDMA_MAPPED_GROUP5 (5U) |
◆ UDMA_MAPPED_GROUP6
| #define UDMA_MAPPED_GROUP6 (6U) |
◆ UDMA_MAPPED_GROUP7
| #define UDMA_MAPPED_GROUP7 (7U) |
◆ Udma_DrvHandle
◆ Udma_ChHandle
◆ Udma_EventHandle
◆ Udma_RingHandle
◆ Udma_FlowHandle