Response for TISCI_MSG_WAKE_REASON.
hdr | TISCI header to provide ACK/NAK flags to the host. |
mode | Mode that was active before wake event. |
reason | Reason the wakeup happened. |
time_ms | Time spent in low power mode. |
Data Fields | |
struct tisci_header | hdr |
char | mode [32] |
char | reason [32] |
uint32_t | time_ms |
struct tisci_header tisci_msg_wake_reason_resp::hdr |
char tisci_msg_wake_reason_resp::mode[32] |
char tisci_msg_wake_reason_resp::reason[32] |
uint32_t tisci_msg_wake_reason_resp::time_ms |