Configures peripherals within the interrupt subsystem according to the valid configuration provided. The following tisci_msg_rm_irq_set_req::valid_params valid bit combinations are allowed: Interrupt Router Mux Configuration - Configures an IR input to output mux connection where the IR input is the src_index and the IR output is the dst_host_irq. Both the src_id and the dst_id must be the device ID of the IR being configured. tisci_msg_rm_irq_set_req::dst_id valid bit == STRUE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == STRUE tisci_msg_rm_irq_set_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_set_req::vint valid bit == SFALSE tisci_msg_rm_irq_set_req::global_event valid bit == SFALSE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == SFALSE Event to VINT Mapping Only - Configure peripheral OES register and add an event mapping to an IA VINT tisci_msg_rm_irq_set_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_set_req::ia_id valid bit == STRUE tisci_msg_rm_irq_set_req::vint valid bit == STRUE tisci_msg_rm_irq_set_req::global_event valid bit == STRUE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == STRUE OES Register Programming Only - Only programs the OES register of the source. Useful for setting UDMAP trigger events and any other events that are not translated to the interrupt domain: tisci_msg_rm_irq_set_req::dst_id valid bit == SFALSE tisci_msg_rm_irq_set_req::dst_host_irq valid bit == SFALSE tisci_msg_rm_irq_set_req::ia_id valid bit == SFALSE tisci_msg_rm_irq_set_req::vint valid bit == SFALSE tisci_msg_rm_irq_set_req::global_event valid bit == STRUE tisci_msg_rm_irq_set_req::vint_status_bit_index valid bit == SFALSE.
hdr | Standard TISCI header |
valid_params | Bitfield defining validity of interrupt route set parameters. The interrupt route set fields are not valid, and will not be used for route set, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for tisci_msg_rm_irq_set_req::dst_id 1 - Valid bit for tisci_msg_rm_irq_set_req::dst_host_irq 2 - Valid bit for tisci_msg_rm_irq_set_req::ia_id 3 - Valid bit for tisci_msg_rm_irq_set_req::vint 4 - Valid bit for tisci_msg_rm_irq_set_req::global_event 5 - Valid bit for tisci_msg_rm_irq_set_req::vint_status_bit_index 31 - Valid bit for tisci_msg_rm_irq_set_req::secondary_host |
src_id | ID of interrupt source peripheral |
src_index | Interrupt source index within source peripheral |
dst_id | SoC IR device ID when the valid_params bits are set to configure an IR mux connection. This field is only valid if TISCI_MSG_VALUE_RM_DST_ID_VALID is set in tisci_msg_rm_irq_set_req::valid_params. |
dst_host_irq | SoC IR output index when the valid_params are set to configure an IR mux connection. This field is only valid if TISCI_MSG_VALUE_RM_DST_HOST_IRQ_VALID is set in tisci_msg_rm_irq_set_req::valid_params. |
ia_id | Device ID of interrupt aggregator in which the virtual interrupt resides. This field is only valid if TISCI_MSG_VALUE_RM_IA_ID_VALID is set in tisci_msg_rm_irq_set_req::valid_params. |
vint | Virtual interrupt number when configuring an interrupt aggregator. This field is only valid if TISCI_MSG_VALUE_RM_VINT_VALID is set in tisci_msg_rm_irq_set_req::valid_params. |
global_event | Global event mapped to interrupt aggregator virtual interrupt status bit. The event is programmed into the OES register of the interrupt source. This field is only applicable for interrupt source's capable of generating global events. This field is only valid if TISCI_MSG_VALUE_RM_GLOBAL_EVENT_VALID is set in tisci_msg_rm_irq_set_req::valid_params. |
vint_status_bit_index | Virtual interrupt status bit to set if the interrupt route utilizes an interrupt aggregator virtual interrupt. The host processor uses the status bit value within the interrupt aggregator vint status register to find the source event which triggered the interrupt. This field is only valid if TISCI_MSG_VALUE_RM_VINT_STATUS_BIT_INDEX_VALID is set in tisci_msg_rm_irq_set_req::valid_params. |
secondary_host | The secondary host value is used to replace the host value for the message that will be sent. This way a message can be sent to configure a different host. For example, if the host is A, and the secondary host is B, then when host A sends a message, the message will be configured for host B, even though host A was the one that sent the message. However, this field is only valid if TISCI_MSG_VALUE_RM_SECONDARY_HOST_VALID is set in tisci_msg_rm_irq_set_req::valid_params. |
Data Fields | |
struct tisci_header | hdr |
uint32_t | valid_params |
uint16_t | src_id |
uint16_t | src_index |
uint16_t | dst_id |
uint16_t | dst_host_irq |
uint16_t | ia_id |
uint16_t | vint |
uint16_t | global_event |
uint8_t | vint_status_bit_index |
uint8_t | secondary_host |
struct tisci_header tisci_msg_rm_irq_set_req::hdr |
uint32_t tisci_msg_rm_irq_set_req::valid_params |
uint16_t tisci_msg_rm_irq_set_req::src_id |
uint16_t tisci_msg_rm_irq_set_req::src_index |
uint16_t tisci_msg_rm_irq_set_req::dst_id |
uint16_t tisci_msg_rm_irq_set_req::dst_host_irq |
uint16_t tisci_msg_rm_irq_set_req::ia_id |
uint16_t tisci_msg_rm_irq_set_req::vint |
uint16_t tisci_msg_rm_irq_set_req::global_event |
uint8_t tisci_msg_rm_irq_set_req::vint_status_bit_index |
uint8_t tisci_msg_rm_irq_set_req::secondary_host |