Request for physical processor control response.
Although this message is essentially empty and contains only a header a full data structure is created for consistency in implementation.
ACK response: The processor access is permitted for the host if processor is un-claimed AND host is permitted to control the processor OR if the host is the recovery master.
NAK response: The processor access is not permitted.
hdr | Generic TISCI message header. |
Data Fields | |
struct tisci_header | hdr |
struct tisci_header tisci_msg_proc_request_resp::hdr |