Request for TISCI_MSG_MIN_CONTEXT_RESTORE.
- Parameters
-
hdr | TISCI header to provide ACK/NAK flags to the host. |
ctx_lo | Low 32-bits of physical pointer to address to use for context restore. |
ctx_hi | High 32-bits of physical pointer to address to use for context restore. |
This message is sent from R5 SPL to TIFS to indicate that DDR is active and TIFS can restore the minimal context from the address provided in the ctx_lo and ctx_hi parameters. This response assumes DDR has been fully restored by R5 SPL before it is sent.