Response for TISCI_MSG_LPM_WAKE_REASON.
hdr | TISCI header to provide ACK/NAK flags to the host. |
wake_source | The wake up source that woke soc from LPM. |
wake_timestamp | Timestamp at which soc woke. |
wake_pin | The pin that has triggered wake up. |
mode | The last entered low power mode. |
rsvd_0 | Reserved for future use. |
rsvd_1 | Reserved for future use. |
Data Fields | |
struct tisci_header | hdr |
uint32_t | wake_source |
uint64_t | wake_timestamp |
uint8_t | wake_pin |
uint8_t | mode |
uint32_t | rsvd_0 |
uint32_t | rsvd_1 |
struct tisci_header tisci_msg_lpm_wake_reason_resp::hdr |
uint32_t tisci_msg_lpm_wake_reason_resp::wake_source |
uint64_t tisci_msg_lpm_wake_reason_resp::wake_timestamp |
uint8_t tisci_msg_lpm_wake_reason_resp::wake_pin |
uint8_t tisci_msg_lpm_wake_reason_resp::mode |
uint32_t tisci_msg_lpm_wake_reason_resp::rsvd_0 |
uint32_t tisci_msg_lpm_wake_reason_resp::rsvd_1 |