Response for TISCI_MSG_LPM_GET_NEXT_SYS_MODE.
hdr | TISCI header to provide ACK/NAK flags to the host. |
mode | The selected system wide low power mode. |
Note: If the mode selection is not yet locked, this API returns "not selected" mode.
Data Fields | |
struct tisci_header | hdr |
uint8_t | mode |
struct tisci_header tisci_msg_lpm_get_next_sys_mode_resp::hdr |
uint8_t tisci_msg_lpm_get_next_sys_mode_resp::mode |