Response for TISCI_MSG_LPM_GET_NEXT_HOST_STATE.
hdr | TISCI header to provide ACK/NAK flags to the host. |
state | The expected state of host in selected low power mode. |
Note: If the mode selection is not yet locked, this API returns invalid state.
Data Fields | |
struct tisci_header | hdr |
uint8_t | state |
struct tisci_header tisci_msg_lpm_get_next_host_state_resp::hdr |
uint8_t tisci_msg_lpm_get_next_host_state_resp::state |