Request for TISCI_MSG_ENTER_SLEEP.
- Parameters
-
hdr | TISCI header to provide ACK/NAK flags to the host. |
mode | Low power mode to enter. |
proc_id | Processor id to be used for restoring boot vector and debug status upon resume. |
core_resume_lo | Low 32-bits of physical pointer to address for core to begin execution upon resume. |
core_resume_hi | High 32-bits of physical pointer to address for core to begin execution upon resume. |
This message is to be sent after TISCI_MSG_PREPARE_SLEEP and actually triggers entry into the previously selected low power mode.