Response for TISCI_MSG_CONTINUE_RESUME.
- Parameters
-
hdr | TISCI header to provide ACK/NAK flags to the host. |
ctx_lo | Low 32-bits of physical pointer to address that was used for context save. |
ctx_hi | High 32-bits of physical pointer to address that was used for context save. |
This response is sent from the DM stub to the TIFS stub to trigger TIFS Stub restore of TIFS context from the address provided in the ctx_lo and ctx_hi parameters. This response assumes DDR has been fully restored by DM Stub before it is sent.