Request for TISCI_MSG_ABORT_ENTER_SLEEP.
hdr | TISCI header to provide ACK/NAK flags to the host. |
This message is sent from the DM firmware to the TIFS firmware during lpm suspend sequence to indicate that DM was not able to successfully suspend the SOC and DM is aborting the sleep cycle. On receiving this message TIFS will wake from WFI and the same message will be forwarded to the power master to wake it from WFI.
Data Fields | |
struct tisci_header | hdr |
struct tisci_header tisci_msg_abort_enter_sleep_req::hdr |