This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for low power modes.
Go to the source code of this file.
Functions | |
int32_t | Sciclient_lpmGetNextSysMode (uint32_t timeout, uint8_t *sysMode) |
Message to get the next system mode. More... | |
int32_t | Sciclient_lpmGetNextHostState (uint32_t timeout, uint8_t *hostState) |
Message to get the next host state. More... | |