AM62x MCU+ SDK  10.00.00

Introduction

This module contains APIs to program and use the QoS. See QoS for more details.

Files

file  qos/v0/qos.h
 This file contains QoS APIs.
 

Data Structures

struct  QOS_Config
 Quality of Service (QoS) configuration structure. More...
 

Functions

void QOS_init (QOS_Config *qosData, uint32_t qosCount)
 QoS Initialization function. More...
 

Function Documentation

◆ QOS_init()

void QOS_init ( QOS_Config qosData,
uint32_t  qosCount 
)

QoS Initialization function.

   Setup the QoS with the given configuration data.
Parameters
qosData[in] Pointer to QoS data array
qosCount[in] Size of the QoS data array