AM62x MCU+ SDK  09.02.01

Detailed Description

TISCI Request for setting DSMEK in SA2UL registers.

Parameters
hdrGeneric TISCI message header.
sa2ul_instanceSA2UL instance number - set to 0
kdf_label_lenLength of "Label" input to KDF
kdf_context_lenLength of "Context" input to KDF
kdf_label_and_context"Label" and "Context" bytes are stored in this array one after another. Maximum length of this field is KDF_LABEL_AND_CONTEXT_LEN_MAX

Data Fields

struct tisci_header hdr
 
uint8_t sa2ul_instance
 
uint8_t kdf_label_len
 
uint8_t kdf_context_len
 
uint8_t kdf_label_and_context [KDF_LABEL_AND_CONTEXT_LEN_MAX]
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_sa2ul_set_dsmek_req::hdr

◆ sa2ul_instance

uint8_t tisci_msg_sa2ul_set_dsmek_req::sa2ul_instance

◆ kdf_label_len

uint8_t tisci_msg_sa2ul_set_dsmek_req::kdf_label_len

◆ kdf_context_len

uint8_t tisci_msg_sa2ul_set_dsmek_req::kdf_context_len

◆ kdf_label_and_context

uint8_t tisci_msg_sa2ul_set_dsmek_req::kdf_label_and_context[KDF_LABEL_AND_CONTEXT_LEN_MAX]