AM62x MCU+ SDK  09.02.01
EPWM_DeadbandCfg Struct Reference

Detailed Description

Structure holding the dead band generation sub-module configuration parameters.

Data Fields

uint32_t inputMode
 
uint32_t outputMode
 
uint32_t polaritySelect
 
uint32_t risingEdgeDelay
 
uint32_t fallingEdgeDelay
 

Field Documentation

◆ inputMode

uint32_t EPWM_DeadbandCfg::inputMode

Input mode control that selects the input source to the falling-edge and rising-edge delay. This can take values from the following enum EPWM_DbInMode_t.

◆ outputMode

uint32_t EPWM_DeadbandCfg::outputMode

Output mode control that selectively enable or bypass the dead-band generation for the falling-edge and rising-edge delay. This can take values from the following enum EPWM_DbOutMode_t.

◆ polaritySelect

uint32_t EPWM_DeadbandCfg::polaritySelect

Polarity selection control that allows selectively invert one of the delayed signals before it is sent out of the dead-band sub-module. This can take values from the following enum EPWM_DbPolSel_t.

◆ risingEdgeDelay

uint32_t EPWM_DeadbandCfg::risingEdgeDelay

Rising edge delay count in cycles.

◆ fallingEdgeDelay

uint32_t EPWM_DeadbandCfg::fallingEdgeDelay

Falling edge delay count in cycles.