AM62x MCU+ SDK  09.02.01

Detailed Description

Parameters for AddrTranslateP_init, this is used by SysConfig and not to be used by end-users directly.

Data Fields

uint32_t numRegions
 
uint32_t ratBaseAddr
 
AddrTranslateP_RegionConfigregionConfig
 

Field Documentation

◆ numRegions

uint32_t AddrTranslateP_Params::numRegions

Number of regions to configure

◆ ratBaseAddr

uint32_t AddrTranslateP_Params::ratBaseAddr

Base address of the RAT HW module

◆ regionConfig

AddrTranslateP_RegionConfig* AddrTranslateP_Params::regionConfig

Pointer to array of region config, number of array element MUST be >= numRegions