AM62x MCU+ SDK
09.02.00
Macros
tisci_devices.h File Reference
Go to the source code of this file.
Macros
#define
TISCI_DEV_CMP_EVENT_INTROUTER0
1U
This file contains:
More...
#define
TISCI_DEV_DBGSUSPENDROUTER0
2U
#define
TISCI_DEV_MAIN_GPIOMUX_INTROUTER0
3U
#define
TISCI_DEV_WKUP_MCU_GPIOMUX_INTROUTER0
5U
#define
TISCI_DEV_TIMESYNC_EVENT_ROUTER0
6U
#define
TISCI_DEV_MCU_M4FSS0
7U
#define
TISCI_DEV_MCU_M4FSS0_CBASS_0
8U
#define
TISCI_DEV_MCU_M4FSS0_CORE0
9U
#define
TISCI_DEV_CPSW0
13U
#define
TISCI_DEV_CPT2_AGGR0
14U
#define
TISCI_DEV_STM0
15U
#define
TISCI_DEV_DCC0
16U
#define
TISCI_DEV_DCC1
17U
#define
TISCI_DEV_DCC2
18U
#define
TISCI_DEV_DCC3
19U
#define
TISCI_DEV_DCC4
20U
#define
TISCI_DEV_DCC5
21U
#define
TISCI_DEV_SMS0
22U
#define
TISCI_DEV_MCU_DCC0
23U
#define
TISCI_DEV_DEBUGSS_WRAP0
24U
#define
TISCI_DEV_DMASS0
25U
#define
TISCI_DEV_DMASS0_BCDMA_0
26U
#define
TISCI_DEV_DMASS0_CBASS_0
27U
#define
TISCI_DEV_DMASS0_INTAGGR_0
28U
#define
TISCI_DEV_DMASS0_IPCSS_0
29U
#define
TISCI_DEV_DMASS0_PKTDMA_0
30U
#define
TISCI_DEV_DMASS0_RINGACC_0
33U
#define
TISCI_DEV_MCU_TIMER0
35U
#define
TISCI_DEV_TIMER0
36U
#define
TISCI_DEV_TIMER1
37U
#define
TISCI_DEV_TIMER2
38U
#define
TISCI_DEV_TIMER3
39U
#define
TISCI_DEV_TIMER4
40U
#define
TISCI_DEV_TIMER5
41U
#define
TISCI_DEV_TIMER6
42U
#define
TISCI_DEV_TIMER7
43U
#define
TISCI_DEV_MCU_TIMER1
48U
#define
TISCI_DEV_MCU_TIMER2
49U
#define
TISCI_DEV_MCU_TIMER3
50U
#define
TISCI_DEV_ECAP0
51U
#define
TISCI_DEV_ECAP1
52U
#define
TISCI_DEV_ECAP2
53U
#define
TISCI_DEV_ELM0
54U
#define
TISCI_DEV_EMIF_DATA_ISO_VD
55U
#define
TISCI_DEV_MMCSD0
57U
#define
TISCI_DEV_MMCSD1
58U
#define
TISCI_DEV_EQEP0
59U
#define
TISCI_DEV_EQEP1
60U
#define
TISCI_DEV_WKUP_GTC0
61U
#define
TISCI_DEV_EQEP2
62U
#define
TISCI_DEV_ESM0
63U
#define
TISCI_DEV_WKUP_ESM0
64U
#define
TISCI_DEV_FSS0
73U
#define
TISCI_DEV_FSS0_FSAS_0
74U
#define
TISCI_DEV_FSS0_OSPI_0
75U
#define
TISCI_DEV_GICSS0
76U
#define
TISCI_DEV_GPIO0
77U
#define
TISCI_DEV_GPIO1
78U
#define
TISCI_DEV_MCU_GPIO0
79U
#define
TISCI_DEV_GPMC0
80U
#define
TISCI_DEV_ICSSM0
81U
#define
TISCI_DEV_LED0
83U
#define
TISCI_DEV_DDPA0
85U
#define
TISCI_DEV_EPWM0
86U
#define
TISCI_DEV_EPWM1
87U
#define
TISCI_DEV_EPWM2
88U
#define
TISCI_DEV_WKUP_VTM0
95U
#define
TISCI_DEV_MAILBOX0
96U
#define
TISCI_DEV_MAIN2MCU_VD
97U
#define
TISCI_DEV_MCAN0
98U
#define
TISCI_DEV_MCU_MCRC64_0
100U
#define
TISCI_DEV_MCU2MAIN_VD
101U
#define
TISCI_DEV_I2C0
102U
#define
TISCI_DEV_I2C1
103U
#define
TISCI_DEV_I2C2
104U
#define
TISCI_DEV_I2C3
105U
#define
TISCI_DEV_MCU_I2C0
106U
#define
TISCI_DEV_WKUP_I2C0
107U
#define
TISCI_DEV_WKUP_TIMER0
110U
#define
TISCI_DEV_WKUP_TIMER1
111U
#define
TISCI_DEV_WKUP_UART0
114U
#define
TISCI_DEV_MCRC64_0
116U
#define
TISCI_DEV_WKUP_RTCSS0
117U
#define
TISCI_DEV_WKUP_R5FSS0_SS0
118U
#define
TISCI_DEV_WKUP_R5FSS0
119U
#define
TISCI_DEV_WKUP_R5FSS0_CORE0
121U
#define
TISCI_DEV_RTI0
125U
#define
TISCI_DEV_RTI1
126U
#define
TISCI_DEV_RTI2
127U
#define
TISCI_DEV_RTI3
128U
#define
TISCI_DEV_RTI15
130U
#define
TISCI_DEV_MCU_RTI0
131U
#define
TISCI_DEV_WKUP_RTI0
132U
#define
TISCI_DEV_COMPUTE_CLUSTER0
134U
#define
TISCI_DEV_A53SS0_CORE_0
135U
#define
TISCI_DEV_A53SS0_CORE_1
136U
#define
TISCI_DEV_A53SS0_CORE_2
137U
#define
TISCI_DEV_A53SS0_CORE_3
138U
#define
TISCI_DEV_PSCSS0
139U
#define
TISCI_DEV_WKUP_PSC0
140U
#define
TISCI_DEV_MCSPI0
141U
#define
TISCI_DEV_MCSPI1
142U
#define
TISCI_DEV_MCSPI2
143U
#define
TISCI_DEV_UART0
146U
#define
TISCI_DEV_MCU_MCSPI0
147U
#define
TISCI_DEV_MCU_MCSPI1
148U
#define
TISCI_DEV_MCU_UART0
149U
#define
TISCI_DEV_SPINLOCK0
150U
#define
TISCI_DEV_UART1
152U
#define
TISCI_DEV_UART2
153U
#define
TISCI_DEV_UART3
154U
#define
TISCI_DEV_UART4
155U
#define
TISCI_DEV_UART5
156U
#define
TISCI_DEV_BOARD0
157U
#define
TISCI_DEV_UART6
158U
#define
TISCI_DEV_USB0
161U
#define
TISCI_DEV_USB1
162U
#define
TISCI_DEV_PBIST0
163U
#define
TISCI_DEV_PBIST1
164U
#define
TISCI_DEV_WKUP_PBIST0
165U
#define
TISCI_DEV_A53SS0
166U
#define
TISCI_DEV_COMPUTE_CLUSTER0_PBIST_0
167U
#define
TISCI_DEV_PSC0_FW_0
168U
#define
TISCI_DEV_PSC0
169U
#define
TISCI_DEV_DDR16SS0
170U
#define
TISCI_DEV_DEBUGSS0
171U
#define
TISCI_DEV_A53_RS_BW_LIMITER0
172U
#define
TISCI_DEV_A53_WS_BW_LIMITER1
173U
#define
TISCI_DEV_GPU_RS_BW_LIMITER2
174U
#define
TISCI_DEV_GPU_WS_BW_LIMITER3
175U
#define
TISCI_DEV_WKUP_DEEPSLEEP_SOURCES0
176U
#define
TISCI_DEV_EMIF_CFG_ISO_VD
177U
#define
TISCI_DEV_MAIN_USB0_ISO_VD
178U
#define
TISCI_DEV_MAIN_USB1_ISO_VD
179U
#define
TISCI_DEV_MCU_MCU_16FF0
180U
#define
TISCI_DEV_CPT2_AGGR1
181U
#define
TISCI_DEV_CSI_RX_IF0
182U
#define
TISCI_DEV_DCC6
183U
#define
TISCI_DEV_MMCSD2
184U
#define
TISCI_DEV_DPHY_RX0
185U
#define
TISCI_DEV_DSS0
186U
#define
TISCI_DEV_GPU0
187U
#define
TISCI_DEV_MCU_MCAN0
188U
#define
TISCI_DEV_MCU_MCAN1
189U
#define
TISCI_DEV_MCASP0
190U
#define
TISCI_DEV_MCASP1
191U
#define
TISCI_DEV_MCASP2
192U
#define
TISCI_DEV_CLK_32K_RC_SEL_DEV_VD
193U
#define
TISCI_DEV_HSM0
225U
#define
TISCI_DEV_MCU_OBSCLK_MUX_SEL_DEV_VD
227U
source
drivers
sciclient
include
tisci
am62x
tisci_devices.h
generated by
1.8.20