AM62x MCU+ SDK  09.02.00
sdl_mcrc_soc.h File Reference

Go to the source code of this file.

Macros

#define SDL_MCRC_INSTANCES   2u
 MCRC instances supported by SOC. More...
 

Enumerations

enum  SDL_MCRC_InstType { MCU_MCRC64_0 = 1U, MCRC64_0 =2U, SDL_MCRC_INVALID = 0xffff }
 MCRC Instance supported. More...
 

Functions

int32_t SDL_MCRC_getBaseaddr (SDL_MCRC_InstType instance, uint32_t *baseAddr)
 This API is used to get the base address of the instance. More...
 

Variables

bool SDL_MCRC_64bit_AtomicWriteSupport [SDL_MCRC_INSTANCES]
 MCRC 64 bit Atomic write support. More...