AM62x MCU+ SDK  09.01.00

Detailed Description

Response to Processor Boot Configuration message.

Although this message is essentially empty and contains only a header a full data structure is created for consistency in implementation.

Parameters
hdrGeneric TISCI message header.

ACK Response: The host had control over the processor and requested operation is successful

NAK Response: The processor access is not permitted or the operation failed.

Data Fields

struct tisci_header hdr
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_proc_set_config_resp::hdr