AM62x MCU+ SDK  09.01.00
sdl Directory Reference

Directories

directory  dcc
 
directory  dpl
 
directory  ecc
 
directory  esm
 
directory  lbist
 
directory  mcrc
 
directory  mtog
 
directory  pbist
 
directory  pok
 
directory  r5
 
directory  rti
 
directory  stog
 
directory  vtm
 

Files

file  sdl_dcc.h [code]
 
file  sdl_ecc.h [code]
 Header file contains enumerations, structure definitions and function.
 
file  sdl_esm.h [code]
 This file contains the SDL ESM API's.
 
file  sdl_exception.h [code]
 Header file contains enumerations, structure definitions and function declarations for SDL EXCEPTION interface.
 
file  sdl_exception_priv.h [code]
 
file  sdl_lbist.h [code]
 
file  sdl_mcrc.h [code]
 
file  sdl_mtog.h [code]
 
file  sdl_pbist.h [code]
 This file contains the SDL PBIST API's.
 
file  sdl_pok.h [code]
 This file contains the prototypes of the APIs present in the device abstraction layer file of POK. This also contains some related macros.
 
file  sdl_rti.h [code]
 
file  sdl_vtm.h [code]
 This file contains the SDL VTM API's.
 
file  sdlr.h [code]
 This file contains the macro definations for Register layer.
 
file  sdlr_tog.h [code]