GPMC Driver API/interface file.
Go to the source code of this file.
Data Structures | |
struct | GPMC_nandCmdParams |
Data structure to set NAND command parameters. More... | |
struct | GPMC_Transaction |
GPMC_Transaction data structure is used with GPMC_transactionInit(), GPMC_nandReadData() and GPMC_nandWriteData(). More... | |
struct | GPMC_Params |
GPMC driver instance parameters. More... | |
struct | GPMC_AddrRegion |
GPMC Address Region. More... | |
struct | GPMC_Object |
GPMC driver object. More... | |
struct | GPMC_timingParams |
GPMC timing parameters. More... | |
struct | GPMC_HwAttrs |
GPMC instance attributes. More... | |
struct | GPMC_Config |
GPMC Driver configuration structure. More... | |
Macros | |
#define | GPMC_CS_TIMING_CONFIG(CSWrOffTime, CSRdOffTime, CSExtDelayFlag, CSOnTime) |
This macro used to make the conf value which is used to configure the CS signal timing configuration. More... | |
#define | GPMC_ADV_TIMING_CONFIG(ADVAADMuxWrOffTime, ADVAADMuxRdOffTime, ADVWrOffTime, ADVRdOffTime, ADVExtDelayFlag, ADVAADMuxOnTime, ADVOnTime) |
This macro used to make the conf value which is used to configure the ADV# signal timing configuration. More... | |
#define | GPMC_WE_OE_TIMING_CONFIG(WEOffTime, WEExtDelayFlag, WEOnTime, OEAADMuxOffTime, OEOffTime, OEExtDelayFlag, OEAADMuxOnTime, OEOnTime) |
This macro used to make the conf value which is used to configure the WE# and OE# signal timing configuration. . More... | |
#define | GPMC_RDACCESS_CYCLETIME_TIMING_CONFIG(rdCycleTime, wrCycleTime, rdAccessTime, pageBurstAccessTime) |
This macro used to make the conf value which is used to configure the read access and cycle time timing configuration. . More... | |
#define | GPMC_CYCLE2CYCLE_BUSTURNAROUND_TIMING_CONFIG(cycle2CycleDelay, cycle2CycleDelaySameCSCfg, cycle2CycleDelayDiffCSCfg, busTAtime) |
This macro used to make the conf value which is used to configure the cycle to cycle and bus turn around time timing configuration. . More... | |
#define | GPMC_DMA_COPY_LOWER_LIMIT (512U) |
size in bytes More... | |
#define | GPMC_CS_BASE_ADDR_SHIFT (24U) |
GPMC CHIP select base address shift value. More... | |
#define | GPMC_ECC_WRAP_MODE1 (1) |
GPMC ECC Wrap mode for ECC value computation. More... | |
#define | GPMC_CMD_INVALID (0xFFFFFFFFU) |
Invalid value for params initialisation. More... | |
GPMC CHIP select | |
Macros which can be used as to select CHIP select instance for GPMC. | |
#define | GPMC_CHIP_SELECT_CS0 (0U) |
#define | GPMC_CHIP_SELECT_CS1 (1U) |
#define | GPMC_CHIP_SELECT_CS2 (2U) |
#define | GPMC_CHIP_SELECT_CS3 (3U) |
GPMC Interupt status flags | |
Macros which can be used as 'interupt' parameter to GPMC_interuptStatusGet, GPMC_interuptStatusClear APIs. | |
#define | GPMC_FIFOEVENT_STATUS (0U) |
#define | GPMC_TERMINALCOUNT_STATUS (1U) |
#define | GPMC_WAIT0EDGEDETECTION_STATUS (2U) |
#define | GPMC_WAIT1EDGEDETECTION_STATUS (3U) |
GPMC Interupt Flags | |
Macros which can be used as 'mode' parameter to GPMC_prefetchPostWriteConfigEnable API. | |
#define | GPMC_FIFOEVENT_INT (0U) |
#define | GPMC_TERMINALCOUNT_INT (1U) |
#define | GPMC_WAIT0EDGEDETECTION_INT (2U) |
#define | GPMC_WAIT1EDGEDETECTION_INT (3U) |
#define | GPMC_PREFETCH_ACCESSMODE_READ (0U) |
#define | GPMC_PREFETCH_ACCESSMODE_WRITE (1U) |
GPMC ECC algorithm | |
Macros which can be used to set GPMC ECC engine algorithm. | |
#define | GPMC_ECC_ALGORITHM_HAMMINGCODE (0U) |
#define | GPMC_ECC_ALGORITHM_BCH (1U) |
GPMC ECC error correvel level. | |
Macros which can be used to set GPMC ECC engine error correction level. | |
#define | GPMC_ECC_BCH_ERRCORRCAP_UPTO_4BITS (0U) |
#define | GPMC_ECC_BCH_ERRCORRCAP_UPTO_8BITS (1U) |
#define | GPMC_ECC_BCH_ERRCORRCAP_UPTO_16BITS (2U) |
GPMC ECC Result Register | |
Macros which can be used to select ECC result register for GPMC ECC engine. | |
#define | GPMC_ECCPOINTER_RESULT_1 (1U) |
#define | GPMC_ECCPOINTER_RESULT_2 (2U) |
#define | GPMC_ECCPOINTER_RESULT_3 (3U) |
#define | GPMC_ECCPOINTER_RESULT_4 (4U) |
#define | GPMC_ECCPOINTER_RESULT_5 (5U) |
#define | GPMC_ECCPOINTER_RESULT_6 (6U) |
#define | GPMC_ECCPOINTER_RESULT_7 (7U) |
#define | GPMC_ECCPOINTER_RESULT_8 (8U) |
#define | GPMC_ECCPOINTER_RESULT_9 (9U) |
GPMC ECC Size Config | |
Macros which can be used to set length of used and unsued bytes in the ECC value. | |
#define | GPMC_ECC_SIZE_0 (0U) |
#define | GPMC_ECC_SIZE_1 (1U) |
GPMC ECC Result Register Size | |
Macros which can be used to set ECC size for ECC result register. | |
#define | GPMC_ECC_RESULT_1 (1U) |
#define | GPMC_ECC_RESULT_2 (2U) |
#define | GPMC_ECC_RESULT_3 (3U) |
#define | GPMC_ECC_RESULT_4 (4U) |
#define | GPMC_ECC_RESULT_5 (5U) |
#define | GPMC_ECC_RESULT_6 (6U) |
#define | GPMC_ECC_RESULT_7 (7U) |
#define | GPMC_ECC_RESULT_8 (8U) |
#define | GPMC_ECC_RESULT_9 (9U) |
GPMC BCH RESULT | |
Macros which can be used to get BCH syndrome polynomial in GPMC_eccBchResultGet API. | |
#define | GPMC_BCH_RESULT0 (0U) |
#define | GPMC_BCH_RESULT1 (1U) |
#define | GPMC_BCH_RESULT2 (2U) |
#define | GPMC_BCH_RESULT3 (3U) |
#define | GPMC_BCH_RESULT4 (4U) |
#define | GPMC_BCH_RESULT5 (5U) |
#define | GPMC_BCH_RESULT6 (6U) |
GPMC CHIP Select SIZE | |
Macros which can be used to set chip select address size. | |
#define | GPMC_CS_MASK_ADDR_SIZE_256MB (0x00U) |
#define | GPMC_CS_MASK_ADDR_SIZE_128MB (0x08U) |
#define | GPMC_CS_MASK_ADDR_SIZE_64MB (0x0cU) |
#define | GPMC_CS_MASK_ADDR_SIZE_32MB (0x0eU) |
#define | GPMC_CS_MASK_ADDR_SIZE_16MB (0x0fU) |
GPMC NAND Specific Timing Parameters | |
Nand flash specific GPMC timing parameters. These are used to GPMC CONFIG registers. | |
#define | GPMC_NAND_CS_ON_TIME 0U |
Chip select on time (FCLK periods) More... | |
#define | GPMC_NAND_WE_ON_TIME 0U |
Write enable on time (FCLK periods) More... | |
#define | GPMC_NAND_ADV_ON_TIME 0U |
Address valid on time (FCLK periods) More... | |
#define | GPMC_NAND_CS_WR_OFF_TIME 6U |
Chip select off time for write (FCLK periods) More... | |
#define | GPMC_NAND_WR_CYCLE_TIME 6U |
Write cycle time (FCLK periods) More... | |
#define | GPMC_NAND_ADV_WR_OFF_TIME 4U |
Address valid off time for write (FCLK periods) More... | |
#define | GPMC_NAND_CS_RD_OFF_TIME 6U |
Chip select off time for read (FCLK periods) More... | |
#define | GPMC_NAND_RD_CYCLE_TIME 6U |
Read cycle time (FCLK periods) More... | |
#define | GPMC_NAND_ADV_AADMUX_ON_TIME 0U |
Address valid on time when using AAD- Muxed protocol. (FCLK periods) More... | |
#define | GPMC_NAND_ADV_AADMUX_RD_OFF_TIME 0U |
Address valid on time for read when using AAD- Muxed protocol. (FCLK periods) More... | |
#define | GPMC_NAND_ADV_AADMUX_WR_OFF_TIME 0U |
Address valid on time for write when using AAD- Muxed protocol. (FCLK periods) More... | |
#define | GPMC_NAND_PAGEBURST_ACCESS_TIME 0U |
Delay between successive words in a multiple access. (FCLK periods) More... | |
#define | GPMC_NAND_OE_ON_TIME 1U |
Output enable on time (FCLK periods) More... | |
#define | GPMC_NAND_OE_OFF_TIME 4U |
Output enable off time (FCLK periods) More... | |
#define | GPMC_NAND_OE_AADMUX_ON_TIME 0U |
Output enable assertion time for the first address phase in an AAD-muxed protocol. (FCLK periods) More... | |
#define | GPMC_NAND_OE_AADMUX_OFF_TIME 0U |
Output enable deassertion time for the first address phase in an AAD-muxed protocol. (FCLK periods) More... | |
#define | GPMC_NAND_ADV_RD_OFF_TIME 4U |
Address valid off time for read (FCLK periods) More... | |
#define | GPMC_NAND_WE_OFF_TIME 3U |
Write enable off time (FCLK periods) More... | |
#define | GPMC_NAND_RD_ACCESS_TIME 4U |
Read access time (FCLK periods) More... | |
#define | GPMC_NAND_C2C_DELAY 0U |
CS high pulse delay (FCLK periods) More... | |
#define | GPMC_NAND_ADMUX_DATA_VALID 0U |
First data write cycle (FCLK) More... | |
#define | GPMC_NAND_WR_ACCESS_TIME 6U |
Write access time (FCLK periods) More... | |
#define | GPMC_NAND_BRST_TAROUND_TIME 0U |
Burst turnaround latency (FCLK periods) More... | |
Typedefs | |
typedef void * | GPMC_Handle |
A handle that is returned from a GPMC_open() call. More... | |
typedef void(* | GPMC_CallbackFxn) (GPMC_Handle handle, GPMC_Transaction *transaction) |
The definition of a callback function used by the GPMC driver when used in GPMC_OPERATING_MODE_CALLBACK mode. More... | |
Enumerations | |
enum | GPMC_nandEccAlgo { GPMC_NAND_ECC_ALGO_NONE = 0x00U, GPMC_NAND_ECC_ALGO_HAMMING_1BIT, GPMC_NAND_ECC_ALGO_BCH_4BIT, GPMC_NAND_ECC_ALGO_BCH_8BIT, GPMC_NAND_ECC_ALGO_BCH_16BIT } |
GPMC ECC engine algoritms. More... | |
enum | GPMC_OperatingMode { GPMC_OPERATING_MODE_BLOCKING = 0, GPMC_OPERATING_MODE_CALLBACK, GPMC_OPERATING_MODE_POLLING } |
GPMC driver operating modes. More... | |
enum | GPMC_TransferMode { GPMC_TRANSFER_MODE_BLOCKING = 0, GPMC_TRANSFER_MODE_CALLBACK } |
GPMC data transfer modes. More... | |
enum | GPMC_TransactionType { GPMC_TRANSACTION_TYPE_READ = 0, GPMC_TRANSACTION_TYPE_WRITE, GPMC_TRANSACTION_TYPE_READ_CMDREG, GPMC_TRANSACTION_TYPE_WRITE_CMDREG } |
Type of the GPMC transaction for read and write. More... | |
enum | GPMC_TransactionStatus { GPMC_TRANSFER_COMPLETED = 0, GPMC_TRANSFER_STARTED, GPMC_TRANSFER_CANCELED, GPMC_TRANSFER_FAILED, GPMC_TRANSFER_CSN_DEASSERT, GPMC_TRANSFER_TIMEOUT } |
Transaction status codes that are set by the GPMC driver. More... | |
Functions | |
static void | GPMC_Params_init (GPMC_Params *params) |
Function to initialize the GPMC_Params struct to its defaults. More... | |
void | GPMC_init (void) |
This function initializes the GPMC module. More... | |
void | GPMC_deinit (void) |
This function de-initializes the GPMC module. More... | |
GPMC_Handle | GPMC_open (uint32_t index, const GPMC_Params *prms) |
This function opens a given GPMC peripheral. More... | |
void | GPMC_close (GPMC_Handle handle) |
Function to close a GPMC peripheral specified by the GPMC handle. More... | |
uint32_t | GPMC_getInputClk (GPMC_Handle handle) |
This function returns the input clk frequency GPMC was programmed at. More... | |
GPMC_Handle | GPMC_getHandle (uint32_t driverInstanceIndex) |
This function returns the handle of an open GPMC Instance from the instance index. More... | |
void | GPMC_writeNandCommandParamsInit (GPMC_nandCmdParams *cmdParams) |
Function to initialise GPMC_nandCmdParams structure to default values. More... | |
int32_t | GPMC_writeNandCommand (GPMC_Handle handle, GPMC_nandCmdParams *cmdParams) |
Function to write NAND command parameters. More... | |
void | GPMC_transactionInit (GPMC_Transaction *trans) |
Function to initialise GPMC_Transaction structure to default values. More... | |
int32_t | GPMC_nandReadData (GPMC_Handle handle, GPMC_Transaction *trans) |
Function to read data from NAND flash using DMA or CPU prefetch/post write engine. More... | |
int32_t | GPMC_nandWriteData (GPMC_Handle handle, GPMC_Transaction *trans) |
Function to write data to NANDflash using CPU prefetch/post write engine. More... | |
int32_t | GPMC_setDeviceSize (GPMC_Handle handle) |
Function to set device width for GPMC instance connected to external device. More... | |
int32_t | GPMC_setDeviceType (GPMC_Handle handle) |
Function to set device type (NANDLIKE OR NORLIKE) for GPMC instance connected to external device. More... | |
int32_t | GPMC_configureTimingParameters (GPMC_Handle handle) |
Function to configure GPMC timing parameters. More... | |
int32_t | GPMC_eccValueSizeSet (GPMC_Handle handle, uint32_t eccSize, uint32_t eccSizeVal) |
Function to set ECC used and unused bytes size in nibbles. More... | |
int32_t | GPMC_eccBchConfigureElm (GPMC_Handle handle, uint8_t numSectors) |
Function to configure ELM module for error correction. More... | |
int32_t | GPMC_eccEngineBCHConfig (GPMC_Handle handle, uint32_t eccSteps) |
Function to configure GPMC ECC engine for BCH algorithm. More... | |
int32_t | GPMC_eccEngineEnable (GPMC_Handle handle) |
Function to enable GPMC ECC engine. More... | |
void | GPMC_eccResultRegisterClear (GPMC_Handle handle) |
Function to clear GPMC ECC result register. More... | |
int32_t | GPMC_eccBchFillSyndromeValue (GPMC_Handle handle, uint32_t sector, uint32_t *bchData) |
Function to fill BCH syndrome value per sector to ELM module. More... | |
int32_t | GPMC_eccBchStartErrorProcessing (GPMC_Handle handle, uint8_t sector) |
Function to start error processing for a sector by ELM module. More... | |
int32_t | GPMC_eccBchCheckErrorProcessingStatus (GPMC_Handle handle, uint32_t sector) |
Function to get error processing status for a sector by ELM module. More... | |
int32_t | GPMC_eccBchSectorGetError (GPMC_Handle handle, uint32_t sector, uint32_t *errCount, uint32_t *errLoc) |
Function to get number of errors per sector by ELM module. More... | |
int32_t | GPMC_eccCalculateBchSyndromePolynomial (GPMC_Handle handle, uint8_t *pEccdata, uint32_t sector) |
Function to compute BCH syndrome polynomial for NAND write operation. More... | |
int32_t | GPMC_eccGetBchSyndromePolynomial (GPMC_Handle handle, uint32_t sector, uint32_t *bchData) |
Function to get BCH syndrome polynomial per sector NAND read operation. More... | |
int32_t | GPMC_configurePrefetchPostWriteEngine (GPMC_Handle handle) |
Function to configure GPMC PREFETCH read and POST write engine. More... | |
int32_t | GPMC_disableFlashWriteProtect (GPMC_Handle handle) |
Function to disable WRITE protect line. More... | |
int32_t | GPMC_enableFlashWriteProtect (GPMC_Handle handle) |
Function to disable WRITE protect line. More... | |
Variables | |
GPMC_Config | gGpmcConfig [] |
Externally defined driver configuration array. More... | |
uint32_t | gGpmcConfigNum |
Externally defined driver configuration array size. More... | |