AM62x SIP is the smallest AM62x module form factor, which integrates high-speed memory, power management, passive components into a single package. All the examples (except SBL) avaiable for am62x-sk can be directly used for SK-AM62-SIP as well. All the SBL examples needs to be changed to use a different DDR configration.
AM62x SIP is packaged with 512MB lpddr, it uses a different DDR configuration file. Download the the AM62x SIP DDR configuration file here, am62x_SIP_ddrReginit-50-800.h.
Update the DDR configuration file for uart_uniflash_stage1 with the path of the file downloaded in STEP 1 - Download AM62x SIP DDR configuration file which is needed to flash application images via the UART.
For all SBL applications, update the DDR configuration file with the file downloaded in STEP 1 - Download AM62x SIP DDR configuration file. For example, in case of sbl_ospi_linux_multistage, DDR driver is included in the sbl_ospi_linux_stage1, update the DDR configuration file .
To build and flash binaries refer EVM Setup and Flash an example application.