AM62x MCU+ SDK  08.05.00
soc.h File Reference

Go to the source code of this file.

Macros

#define SOC_BOOTMODE_MMCSD   (0X36C3)
 Switch value for SD card boot mode. More...
 
SOC Domain ID

#define SOC_DOMAIN_ID_MAIN   (0U)
 
#define SOC_DOMAIN_ID_MCU   (1U)
 
#define SOC_DOMAIN_ID_WKUP   (2U)
 

Functions

int32_t SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable)
 Enable clock to specified module. More...
 
int32_t SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
 Set module clock to specified frequency. More...
 
const char * SOC_getCoreName (uint16_t coreId)
 Convert a core ID to a user readable name. More...
 
void SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition)
 Lock control module partition to prevent writes into control MMRs. More...
 
void SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition)
 Unlock control module partition to allow writes into control MMRs. More...
 
uint64_t SOC_getSelfCpuClk (void)
 Get the clock frequency in Hz of the CPU on which the driver is running. More...
 
int32_t SOC_moduleGetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t *clkRate)
 Get module clock frequency. More...
 
void SOC_setDevStat (uint32_t bootMode)
 Change boot mode by setting devstat register. More...